STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to use FreeRTOS in a static library

STM32H747XICubeIDECubeMXCubeProgrammerWindows 11I am building a static library that will be used by both CM7 and CM4 cores. I have enabled FreeRTOS for each core. How do I link FreeRTOS into my static library?

rtalan by Associate III
  • 1559 Views
  • 1 replies
  • 0 kudos

Activate preload register for HRTIM in push-pull mode

Hi,Recently, I'm studying HRTIM with G4 product. It's known there's a push-pull logic in HRTIM which could output CHx1 and CHx2 alternately to achieve balanced output. I could generate the setting from CubeMX and get push-pull waveform as I wanted. H...

Syl by Associate
  • 936 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G4 ADC MULTICHANNEL DMA

I'm trying to read ADC2 IN1(PA0 connected to GND) and ADC2 IN2 (PA1 connected to 3.3V). static void MX_ADC2_Init(void) { /* USER CODE BEGIN ADC2_Init 0 */ /* USER CODE END ADC2_Init 0 */ ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE ...

Ethernet for U-BOOT on STM32H753i-EVAL2

Hi,I have the STM32H753i-EVAL2 and need to boot from TFTP using U-BOOT. As the STM32H743i-EVAL is very similar to STM32H753i-EVAL2, I uses the stm32h743-eval_defconfig configuration in U-BOOT. I also added the- Networking support- Synopsys Designware...

technicr by Associate
  • 1418 Views
  • 0 replies
  • 0 kudos

Resolved! Ethernet stops working on H7 dual core

Hi there!I 've got a project where i use the STM32H757 dual core (Riverdi 7")the M7 core runs freeRTOS with Ethenet (ping and echo OK)the M4 coreruns freeRTOS with ADC  using DMA and some EXTI (working as expected)When starting the M7 core first and ...

PGrif.2 by Associate III
  • 4724 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.