STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H5 Waveform Generation using External DAC

Hi,I am trying to generate waveforms using the STM32H563 microcontroller and several AD5791 DAC ICs. I am using the ADG732 Multiplexer with 5 select lines to connect my CS line to the required DAC IC. A simplified image of the hardware is provided be...

DAC_WF.jpg Screenshot 2024-06-11 125201.png mrsthb_qmt_0-1718274366194.png mrsthb_qmt_0-1718277565482.png

SD Card R/W error with Olimex STM32-E407 board

Hi, I am using Olimex STM32-E407 evaluation board which has STM32F407ZG. I tried Freertos,LWip etc successfully. But when i tested SD card interfaced with SDIO, i got errors. Failed to mount SD Card. I am attaching the main.c file herewith. Kindly he...

IBIS model Configuration STM32U5A9

Greetings,   I have a question regarding the IBIS model of STM32U5A9 family. in the setup of any pin there is model parameter that has to be selected. There are several models such as io100m_ls_xx_xxx. what exactly those models mean in terms of actua...

Au by Associate
  • 1351 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 QUADSPI clock configuration

I have question about STM32H7 QUADSPI clock configuration.It seems STM32H7 contains two different source clocks.If I select HCLK3 as the clock source for the QUADSPI Clock Mux, how is the QUADSPI clock frequency calculated? Regardless of selecting HC...

nonoriri_0-1718245025308.png nonoriri_1-1718245090453.png
nonoriri by Associate III
  • 3420 Views
  • 3 replies
  • 2 kudos

Resolved! Switching between UART to GPIO and GPIO to UART

Hi     i am configuration UART1 as default and Tx pin switching into GPIO then  reset (Low) the GPIO for 28 micro sec(delay)  and set(high) the GPIO then again switching to UART1. during switching waveform level  is intermediate as show in below. (my...

Naresh_ by Associate III
  • 3865 Views
  • 4 replies
  • 3 kudos

STM32U5 Nucleo where to find demo source code

Hi community people, As an introduction, please note I'm completely new to the STM32 world, and back in embedded world after a long break in the application level. I now jump in a new project that will be based on a STM32U5, and I start digging in do...

PatriceL by Associate III
  • 3730 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.