cancel
Showing results for 
Search instead for 
Did you mean: 

Own STM32F4 Board .. whats with VCAP1 and PDR_on Pin?

deeksha23jan
Associate

Hi can I leave PDR_ON pin as No Connect for STM32F46x LQFP208 and VBAT connected to VDD. Not really using the Internal reset function.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

PDR_ON does not have any internal pullup or pulldown, so it must be connected to either VDD or VSS.

> Not really using the Internal reset function.

So, do you have an external reset chip to rely on?

JW

PS. Don't hijack threads, especially if they are 12 years old. Start your own and discuss there.