STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN failed to reinit after deinit for STM32F105

Can failed to reinit after deinit. 1. Two cans was used for my projects which was generated by stm32cubemx 2. after run for a short while , I turn off both cans by HAL_CAN_DeInit 3. then I reinit both cans by MX_canx_init and found it failed in HAL_C...

supgz_0-1720093361327.png
supgz by Associate II
  • 2410 Views
  • 4 replies
  • 0 kudos

PH3/BOOT0 pin on the STM32L432KC

May I know where is the PH3/BOOT0 pin on the STM32L432KC board? I don't see any GPIO pin for that. It is connected to the F103 chip onboard but how do I use that?

Abijith by Associate II
  • 2593 Views
  • 4 replies
  • 0 kudos

Resolved! STM32U575/585 MSIS calibrated by LSE question

If the LSE 32.768KHz crystal is disturbed after the system starts with MSIS auto calibration, and the MSIS clock is used by the PLL for the SYSCLK, the frequency of SYSCLK loses its 0.25% accuracy and starts to drift.Is there any register or interrup...

JoshA by Associate
  • 1534 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H730 outside of program code

Hello!I'm porting a working code from H750VB to H730VB, generating a new HAL core from STM32CubeMX, but right after entering on "SystemClock_Config" function at debug mode, I've got the message "Break at address 0x46bd3718 with no debug information a...

Peaga by Senior
  • 9495 Views
  • 18 replies
  • 9 kudos

Resolved! STm32CubeMX bug: CAN2 wrong configuration

Posted on June 26, 2014 at 16:31 Hi, I tried to configure my STm32F207 using the ''Cube'' to use the CAN2 and I found a bug. This is the initialization code generated by the ''Cube'': void HAL_CAN_MspInit(CAN_HandleTypeDef* ...

Resolved! Same project, two different ioc files

I have a working project with its .ioc file.Now I need to port the project codebase to another project that uses exactly the same processor, but with different pinout: the peripherals in the project will be the same, mapped on some other pins.I need ...

Resolved! Cannot uncheck "save power of non-active UCPD" in ioc

Hey All, I cannot seem to uncheck the option "save power of non-active UCPD - deactive Dead Battery pull-up" Everytime I generate code I have to manually comment out (disable) (HAL_SYSCFG_StrobeDBattpinsConfig(SYSCFG_CFGR1_UCPD1_STROBE | SYSCFG_CFGR1...

Screenshot 2024-04-01 091533.png
s_bhonwal by Associate II
  • 2709 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.