STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX: Cannot disable Systick INT

Posted on April 13, 2014 at 13:46Hello! When using CubeMX and going to Configuration and System --> NVIC ''System tick timer'' Interrupt is enabled. When I disable it, click apply and ok and then open NVIC dialog again it's enabled instead of disabl...

Resolved! Minimal FMAC gives wrong answer on STM32G4

I have the FMAC working enough to produce values readable from RDATA, but they are acting strangely and giving small positive and negative values and 0. As a minimal test, I created the below code to have X1 and X2 be all 1s. A buffer length of 18 sh...

KHarb.1 by Senior II
  • 1570 Views
  • 1 replies
  • 0 kudos

Resolved! HAL_Delay() doesn't synch with RTC on STM32H7A3

I'm rewriting some of my old LL code to use HAL and having trouble getting the RTC to read time correctly. I have a simple test project where I'm calling HAL_RTC_GetTime() and HAL_RTC_GetDate() before and after a call to HAL_Delay() with the expectat...

magene_2-1720213155288.png magene_0-1720212267571.png magene_1-1720212325661.png
magene by Senior II
  • 2094 Views
  • 2 replies
  • 0 kudos

Resolved! 32F413 Port Pin States During Deep Sleep?

I'm the hardware guy on a 32F413 project where we have a lot of impulse noise nearby on the PCB.  Because of this I've been on a campaign to make certain that all microcontroller I/O pins are equipped with pull-up or pull-down resistors.The project h...

JOLSO.11 by Associate II
  • 1587 Views
  • 1 replies
  • 0 kudos

Resolved! my stm32f4 cannot connect to stlink normally

I am facing an issue with my custom-made STM32F4x minimum system board. I am experiencing unstable connections with the STLink. I am using an AMS1117 for power supply, and I have found that when the STLink supplies power at 5V to the AMS1117, it cann...

Resolved! FileX + USB Host on B-U585I-IOT02A

Hello forumI'm trying to implement a project that takes the sensor data and saving it into a USB flash Drive,for that, I'm trying to use the MX system to activate:USBPD - Type C only, TIM2, enabled USB support USBX - Host CoreStack FS, Host Controlle...

External 32.768KHz Oscillator for RTC in STM32H743

Hi,I want to use External 32.768KHz Oscillator as clock source for RTC. This is a reference schematic how I intend to connect Oscillator with RCC_OSC32_IN pin on my STM32H743 microcontroller.  My Query is since oscillator requires Vcc 3.3V to operate...

VShet2_0-1720246581771.png
VShet.2 by Associate III
  • 3380 Views
  • 3 replies
  • 0 kudos

Problems with communication with TMC2209 through UART

Hello. I have problems with communication with TMC2209 through UART. It doesn't respond at all. I think that I've fried a receiver in UART1. Is that even possible? My board is Nucleo-F303k8. Please help me. Here's the code:/* USER CODE BEGIN Header *...

Adar70 by Associate II
  • 4530 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.