STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STMG0 Multichannel ADC CubeIDE configuration issue

Hi,I'm not able to set the STM32G030C6 ADC1 for 9 + Internal Temperature Sensor channels. Here's my ADC1 Mode and Configuration parameters I'm using this recently updated Software Package VersionSTM32CubeG0 Firmware Package V1.6.2Does anyone know wha...

Gaston_1-1719938564685.png Gaston_2-1719938744194.png
Gaston by Senior
  • 2203 Views
  • 3 replies
  • 0 kudos

Sampling frequency issue

Hello,I am using an STM32U585CIU6 with LSM6DSOX to sample acceleration values, in order to use it in a project on NanoEdge. I am facing an issue while trying to sample higher frequencies. My accelerometer is set to operate at 833Hz. By printing the n...

STM32 NUCLEO-H743ZI2 UART Baud rate mismatch problem

Currently i am working with nucleo-h743zi2 board. I set the Baud rate in CubeMx to 115200. In the Hercules program, when I set the baud rate to 115200, the data does not flow correctly, but when I set the baud rate to 38400, it flows correctly. Why m...

uart.PNG
Chaotic by Associate II
  • 4042 Views
  • 7 replies
  • 2 kudos

Resolved! getting stuck into hard fault handler

i am using stm3210e eval board. It has NAND flash memory of 512 Mbit and I am trying to read data from it but it gets inside hard fault handler. although i am able to read the device IDBelow is the codeNAND_IDTypeDef nand[1]; HAL_NAND_Read_ID(&hnand1...

Screenshot 2024-06-24 162932.png
rahul7515 by Associate III
  • 1460 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H730ZB - OCTOSPI - cannot write DCR1 register

Hi,On a custom board using STM32H730ZB, I try to use QUAD SPI flash memory.Here is the CubeMX config :In MX_OCTOSPI1_Init function, I break on HAL_SPI_INIT functionThis function come from pack STM32H7 version 1.11.2In line #415 of stm32h7xx_hal_ospi....

COSEBE_0-1719322210622.png Capture d’écran 2024-06-25 153034.png Capture d’écran 2024-06-25 154518.png
COSEBE by Senior
  • 1632 Views
  • 5 replies
  • 1 kudos

Resolved! STM32G474RET FDCAN Tx FIFO free level always be 0

1. [Part Number] STM32G474RET2. [Environment] CubeMx on custom board3. [Schematics] NA4. [Details]  The function "HAL_FDCAN_GetTxFifoFreeLevel"  always return 0, Tx FIFO cant be cleaned, but my can bus is in error-active status, TEC is 0, REC is 0 5....

eason_Yi by Associate II
  • 1840 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G0 FDCAN reception interrupt doesn't trigger

Hello everyone, I'm a beginner in the FDCAN field with STM32. I'm trying to establish communication between two custom boards equipped with the same CAN transceiver. The mode is normal FDCAN. Here's the configuration of the FDCAN module for completen...

seba21 by Associate II
  • 3098 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.