STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5G7VJT6Q - 5V-tolerant pins (FT_h) for Hall encoder

Hi,MCU planned to use - STM32U5G7VJT6QPlanning to use PD12,PD13,PE0,PE3,PC7,PE5 as encoder and hall sensor pins as shown below in the image.But these signals are 5V logic. Is it okay if we give 5V to these pins?In datasheet it is mentioned as 5V tole...

NIVI_0-1720192131454.png
NIVI by Associate III
  • 3629 Views
  • 5 replies
  • 0 kudos

Flash memory protection in STM32G0B1

Hi Team,MCU: STM32G0B1Requirement: Flash memory protection is needed for the MCU code.I am using stm32g0b1 MCU for my project, where I have completed my development activities.MCU Flash contains two things. 1) MCU code 2) other important data related...

Dthum.1 by Associate III
  • 2355 Views
  • 2 replies
  • 0 kudos

about PC14,PC15

I use STM32F030C8T6 recently, and uses GPIOC14,GPIOC15 as input(include interrupt,to wake up STOP MODE); Before IAP,program running correct,GPIO14 and GPIO15 wake up the program correctly. But when I use IAP to download the program,and jump to run it...

STM32F410 RM DMA table contains nonexistent DAC2

Also, the only DAC pin marking is so sloppy that this can be found on one single page:I'd recommend to go through all DAC-containg DSs and RMs and unify nomenclature. It's okay (and IMO preferrable) to call the single DAC module DAC1 and its single p...

waclawekjan_0-1720344488338.png waclawekjan_1-1720344682217.png

L9961 G071RB is dead ? how can I revive it ?

dear St:my L9961 seems dead :I can not drag new file to g071RB, it shows that the space is not enough; also a new file Fail.txt showd up: ”The interface firmware failed to reset/halt the target MCU”; How can I revive my MCU ? 

jingbos by Associate II
  • 1420 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.