STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube-AI Software Pack Utilization Problem

Unsure if this has been answered before, however, upon activating the Cube-AI Core and application software pack, the remains static, ie it stays blacked out with a gear icon next to it referring me back to the software packs screen, which already sh...

jdudley9_0-1770405548437.png jdudley9_1-1770405580305.png
jdudley9 by Associate
  • 330 Views
  • 3 replies
  • 0 kudos

Resolved! Stm32l552 event wakeup pin

I am using stm32l552zetxq. I am testing standbymode with wakeup from event. According to reference manual RM0438, there are 5 wake up pin to wake up the mcu from standby/shutdown mode wkup1 to 5 with polarity setting option in PWR_CR3 and PWR_CR4. Bu...

sourav by Associate II
  • 328 Views
  • 2 replies
  • 0 kudos

STM32F303CBT6 DAC not working with DMA

Dear all,I'm trying to generate a waveform using DAC OUT1.I configured pin PA4 as analog (works)I configured DAC1 without DMA and it worksI configured TIM6 and it works Then I configured DAC with DMA, configured DMA, but output never changes.Where ca...

Resolved! STM32G474 – TIM_ETR to tim_trgo

Hello,I may have made a *** of myself on a prototype, and need a bit of help with a work-around. I have an external clock signal on TIM20_ETR (PG5) for some pulse counting stuff. This works.However, I intended to use the same clock signal to trigger ...

EThom.3 by Senior III
  • 401 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.