STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 NUCLEO - GPIO fault

Board: NUCLEO-N657X0-QRevision: CProblem: MCU cannot pull PA2 to low, only to about 2.5V. I tried it in push-pull and open drain modes. SB6 has been desoldered to isolate it from the analog attenuation circuit, but it didn't work with it soldered. It...

Resolved! SPI DMA transmit complete interrupt to early

Hello,I have an STM32G441 and using DMA to transmit some SPI data. All works so far. The problem is the chipselect. I am using the software chipselect. So before I start the DMA I pull CS low. Then when the DMA complete interrupt fires I pull it high...

Resolved! internal behavior of the NRST pin on STM32H563ZIT6 ?

Hello,I am currently reviewing a hardware design based on the STM32H563ZIT6 and have some questions regarding the internal and external behavior of the NRST pin.My main question is how the NRST pin operates specifically during an NVIC_SystemReset.Cur...

leejunggyun_1-1770359431004.png leejunggyun_6-1770359931331.png leejunggyun_2-1770359545339.png leejunggyun_3-1770359722188.png

Resolved! FDCAN RAM allocation on STM32G4 series

May I ask how the FDCAN Message RAM offset allocation,  Tx and Rx BufferElementSize can be configured on G4 Series. As in cubeMX it doesnt give me the option to like the H7 series. Or is that done automatically by the core when generating the code?If...

Qin1 by Associate III
  • 522 Views
  • 3 replies
  • 2 kudos

STM32L051C8 comparator consumption

Hi,I have a strange problem on an STM32L051C8 with the comparators enabled in window mode.If I put the system in stop about 20 seconds after powering the microcontroller, the current draw is about 250 uA. If I then exit the stop mode with a soft rese...

Ufoit by Associate II
  • 392 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.