STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! H7x3 SAI with DMA in MONO mode

Heyho,using all SAI blocks on H723 / H733 / H735 with stereo audio ADCs via DMA, working smoothly as long as both channels are used.Now I wanted to implement turning off single channels, and I thought I could do that with the SAI / DMA settings.I jus...

LCE by Principal II
  • 4132 Views
  • 7 replies
  • 0 kudos

uart2 not working in stm32 nucleo F411RE

Hi,i wrote code that wait for a ping from esp32 and when he got it, it sent back pong to esp32In the uart1 everthing works fine, but i do not understand why, in uart2 it is not workingI doubled checked the code and everthing looks ok for me,  The cod...

roystm321 by Associate III
  • 5801 Views
  • 13 replies
  • 0 kudos

GPIO_Output

Hello St-communityI am working on stm32g030c6t6 MCU When i have select PB11 PA7 and PA5 has GPIO_OUTPUT it is giving issue in flashing programPlease tell me solution 

snehadakhare01_0-1729056692222.png

Not able to update option bytes

Hi All,I am working on STM32H743VITx. Somehow by mistake "readout protection" is being on. RDP level has set to 1. I am trying to set it 0 by ST-Lint utilities (GUI & STM32Programmer both tried). but the message ''Could not set Option bytes!'' appear...

Tabrez by Associate
  • 3108 Views
  • 4 replies
  • 0 kudos

Compress JPEG fail at jpeg_set_default

Hi,I am a newbie and trying to compress RGB image data to JPEG and save to SD card. Step by step I monitor the debugging of CubeMX, which is very useful to me. And finally I see it can not pass the jpeg_set_default() function due to "out of memory", ...

ULOK by Associate II
  • 2177 Views
  • 2 replies
  • 0 kudos

STM32U5 hspi fifo

Greetings!I'm working with an STM32U5G9 processor, trying to communicate to a HyperBus psram over the hspi peripheral.  My initial simple test is to try to do an indirect read of the psram 16 bit id register at register space address 0.I am capturing...

rdl_42 by Associate III
  • 2556 Views
  • 4 replies
  • 0 kudos

Option Bytes to RDB level 2

I am using Segger JLINK for software downloading to below boards. After downloading software, there is need to enable RDL level 2. Kindly give support below platforms.STM32L562VET6STM32L552VET6STM32L552CCT6Edit: I am using SEGGER J-Flash for software...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.