2024-10-01 12:13 AM - last edited on 2024-10-01 2:00 AM by mƎALLEm
Hi
i am using stm32f767IGK6 i am able to write data in nor flash but can't read data of same address.
by use this APIs HAL_QSPI_Transmit(), HAL_QSPI_Receive()
Regard & Thanks,
Naresh
2024-10-01 1:02 AM
Hello @Naresh_ ,
Could you please give more detail about the issue.
Are you read data in memory mapped mode or indirect mode?
Could you please take a look at the errata sheet precisely:
May QSPI_ReadWrite_IT this example can help you.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-01 2:13 AM
Your presentation of the problem and the context is inadequate. Try harder as if you're explaining to someone who's not physically watching you code and test the issue.
2024-10-16 2:48 AM
Hi ,
Now i am able to Read Manufacturer ID and the Device ID Nor flash by using below code
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = S25FL128S_READ_ID_CMD;//0x90 or 0x9f
s_command.Address = QSPI_ADDRESS_NONE;
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE;
s_command.NbData = 3;
s_command.DummyCycles = 0;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
/* Configure the command */
if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
/* Reception of the data */
if (HAL_QSPI_Receive(Ctx, ID, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
when i am trying read nor flash then based data lines it change data like 255, 81.. as below showing code
s_command.AddressSize = QSPI_ADDRESS_32_BITS;
s_command.Address = ReadAddr;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.NbData = Size;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
/* Configure the command */
if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
/* Reception of the data */
if (HAL_QSPI_Receive(Ctx, pData, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
when i trying to write enable and write then it is not working can please help
i send instruction is 0x6 for write enable then it send error at this API's is HAL_QSPI_AutoPolling() time issue
QSPI_CommandTypeDef s_command;
QSPI_AutoPollingTypeDef s_config;
UNUSED(Mode); /* The command Write Enable is always 1-0-0 */
/* Enable write operations */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = S25FL128S_WRITE_ENABLE_CMD;
s_command.Address = QSPI_ADDRESS_NONE;
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_1_LINE; // changed to 0 data to l data line
s_command.DummyCycles = 0;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(Ctx, &s_command, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
/* Configure automatic polling mode to wait for write enabling */
s_config.Match = S25FL128S_SR1_WREN;
s_config.Mask = S25FL128S_SR1_WREN;
//s_config.MatchMode = QSPI_MATCH_MODE_AND;
s_config.MatchMode = QSPI_MATCH_MODE_OR;
s_config.StatusBytesSize = 1;
//s_config.Interval = 0x10;
s_config.Interval = 0xFF;
s_config.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
s_command.Instruction = S25FL128S_READ_STATUS_REG1_CMD;
s_command.DataMode = QSPI_DATA_1_LINE;
if (HAL_QSPI_AutoPolling(Ctx, &s_command, &s_config, HAL_QSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return S25FL128S_ERROR;
}
HAL_StatusTypeDef HAL_QSPI_AutoPolling(QSPI_HandleTypeDef *hqspi, QSPI_CommandTypeDef *cmd, QSPI_AutoPollingTypeDef *cfg, uint32_t Timeout)
{
HAL_StatusTypeDef status;
uint32_t tickstart = HAL_GetTick();
/* Check the parameters */
assert_param(IS_QSPI_INSTRUCTION_MODE(cmd->InstructionMode));
if (cmd->InstructionMode != QSPI_INSTRUCTION_NONE)
{
assert_param(IS_QSPI_INSTRUCTION(cmd->Instruction));
}
assert_param(IS_QSPI_ADDRESS_MODE(cmd->AddressMode));
if (cmd->AddressMode != QSPI_ADDRESS_NONE)
{
assert_param(IS_QSPI_ADDRESS_SIZE(cmd->AddressSize));
}
assert_param(IS_QSPI_ALTERNATE_BYTES_MODE(cmd->AlternateByteMode));
if (cmd->AlternateByteMode != QSPI_ALTERNATE_BYTES_NONE)
{
assert_param(IS_QSPI_ALTERNATE_BYTES_SIZE(cmd->AlternateBytesSize));
}
assert_param(IS_QSPI_DUMMY_CYCLES(cmd->DummyCycles));
assert_param(IS_QSPI_DATA_MODE(cmd->DataMode));
assert_param(IS_QSPI_DDR_MODE(cmd->DdrMode));
assert_param(IS_QSPI_DDR_HHC(cmd->DdrHoldHalfCycle));
assert_param(IS_QSPI_SIOO_MODE(cmd->SIOOMode));
assert_param(IS_QSPI_INTERVAL(cfg->Interval));
assert_param(IS_QSPI_STATUS_BYTES_SIZE(cfg->StatusBytesSize));
assert_param(IS_QSPI_MATCH_MODE(cfg->MatchMode));
/* Process locked */
__HAL_LOCK(hqspi);
if(hqspi->State == HAL_QSPI_STATE_READY)
{
hqspi->ErrorCode = HAL_QSPI_ERROR_NONE;
/* Update state */
hqspi->State = HAL_QSPI_STATE_BUSY_AUTO_POLLING;
/* Wait till BUSY flag reset */
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_BUSY, RESET, tickstart, Timeout);
if (status == HAL_OK)
{
/* Configure QSPI: PSMAR register with the status match value */
WRITE_REG(hqspi->Instance->PSMAR, cfg->Match);
/* Configure QSPI: PSMKR register with the status mask value */
WRITE_REG(hqspi->Instance->PSMKR, cfg->Mask);
/* Configure QSPI: PIR register with the interval value */
WRITE_REG(hqspi->Instance->PIR, cfg->Interval);
/* Configure QSPI: CR register with Match mode and Automatic stop enabled
(otherwise there will be an infinite loop in blocking mode) */
MODIFY_REG(hqspi->Instance->CR, (QUADSPI_CR_PMM | QUADSPI_CR_APMS),
(cfg->MatchMode | QSPI_AUTOMATIC_STOP_ENABLE));
/* Call the configuration function */
cmd->NbData = cfg->StatusBytesSize;
QSPI_Config(hqspi, cmd, QSPI_FUNCTIONAL_MODE_AUTO_POLLING);
/* Wait until SM flag is set to go back in idle state ***** */
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_SM, SET, tickstart, Timeout);
if (status == HAL_OK)
{
__HAL_QSPI_CLEAR_FLAG(hqspi, QSPI_FLAG_SM);
/* Update state */
hqspi->State = HAL_QSPI_STATE_READY;
}
}
}
else
{
status = HAL_BUSY;
}
/* Process unlocked */
__HAL_UNLOCK(hqspi);
/* Return function status */
return status;
}
status = QSPI_WaitFlagStateUntilTimeout(hqspi, QSPI_FLAG_SM, SET, tickstart, Timeout); i am fail to check the status register of nor flash.
how to do write_enable , write operation in nor flash?
Regards & Thanks,
Naresh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.