STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No price info on STM32 selector??

Hi,I tried CubeIDE as well as the online STM32 selector but it seems that there is no price information in the results?Did I miss something?The distributors (Digikey, Mouser etc) don't list all peripherals in a parametric form as refined as ST (obvio...

Ricko by Senior III
  • 5236 Views
  • 10 replies
  • 12 kudos

stm32f767bi and lan8720a

Hello everybody!I'm working with MCU stm32f767bi and I'm trying to communicate a ethernet port (lan8720a).I'm using a MXcube32 to configure the ETH and LWIP, but I can't get work the port.If someone has experience integrating this two devices please ...

LeoGP by Associate II
  • 2359 Views
  • 4 replies
  • 0 kudos

Resolved! STM32G4 W25Q128JVSIQ page program issue.

Hello. I am using W25Q128JVSIQ for flash storage. I am curious if anyone has run into this or a similar issue with using the flash chip with standard SPI.1: I can program page 0 up to 256 bytes without issues.2: I can then program page 1 up to 255 by...

STM32G4_SPI_FLASH.png
joe31093 by Associate II
  • 3233 Views
  • 3 replies
  • 0 kudos

stm32h503rbxx upload error

Hi,I would like to upload a program to h503rbt6 version stm32 chip but having trouble. I' m using a bare chip by using a dip converter and jumper cables. Earlier I've tested the same method and no problem observed. Below is the output of the upload w...

STM32G0 TX Busy Flag Set when ClockPrescaler is 8

Hi, HAL_UART_STATE_BUSY_TX is always Set when I change the ClockPrescaler of USART Paremeter.My Cube configurations are in photo above. I have to drive Usart with 100 Baudrate. Systemclock Frequency is 50Mhz.  When SystemClock is 50Mhz and ClockPresc...

gceti1_0-1728306451623.png gceti1_1-1728306542177.png
gceti.1 by Associate II
  • 2167 Views
  • 4 replies
  • 0 kudos

STM32G474 HRTimer, Dead time And Duty Cycle

Hi all! Hoping someone can help me with this. Right now, I have Timer A and Timer B as my main outputs; Timer A controls one set of switches in my half bridge, and Timer B controls the other half. I have one "mode" set, where I can adjust the phase s...

Jbin0101 by Associate III
  • 3311 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.