STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Internal temperature sensor

Posted on July 02, 2011 at 20:18Hello.I'm trying to use the internal temperature sensor, but I can't understand the reference manual formula:  Temp = ((V25 - Vsense) / Avg_slope) + 25).In the product datasheet, it says V25 is 1.41 V and Avg_slope is...

Recover ST-LINK firmware

Posted on September 07, 2012 at 14:29Hi, I would like to know if its posible to restore st-link firmware on the STM32F103C8. I have 2 boards and I tried to program it to play a little with USB. Can I restore it? How? Thanks in advance.

rmarku by Associate
  • 1372 Views
  • 1 replies
  • 0 kudos

HSERDY bit is always 0

Posted on September 08, 2012 at 14:48Hi guys, I have a board from hardware guys who told me they had tested this board and everything is fine including SPI1. But I cannot let my SPI1 working because status register bit TXE is always 0. From the spec...

UART4 Rx

Posted on September 10, 2012 at 04:03Hello every1, few days ago i had a problem with uart tx and nw i have solved that problem. so my tx is working fine now. my rx is working too but very slow and gets junk values. below is my code. int main(void) {...

vivek2 by Associate II
  • 2234 Views
  • 4 replies
  • 0 kudos

how to update TIM_Period when timer i running

Posted on September 09, 2012 at 21:55Hi I need to be able to update the Period for a timer (TIM3) I though it was simple, but no.I have tried :else if(TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET){ ledTimeBaseStructure.TIM_Period = newValue; TIM_Ti...

spa23 by Associate III
  • 828 Views
  • 1 replies
  • 0 kudos

Is it possible to use i2c in a full duplex mode?

Posted on September 07, 2012 at 08:09Hi! all,Is it possible to use i2c of stm32l152rbt6 in a full duplex mode? if so can you post/send me the relevant code for that.thanks,  #i2c-in-a-full-duplex-mode #i2c-fundamentals

STM32F103 Download Hex File Using Command Line

Posted on September 07, 2012 at 09:12Hello,I want to download hex file to STM32F103 using STMFlashLoader.exe. But I haven't been successul yet. Do you have sample command with work STM32F103? It's very useful for me to understand command line.Thank ...

MB1034B STM32F0DISCOVERY problem on UART1 PA10

Posted on September 07, 2012 at 09:01I'm using STM32F0DISCOVERYI can't receive any char on UART, no interrrupt!Here my initialization:&sharpdefine RCC_PORT_RX RCC_AHBPeriph_GPIOA&sharpdefine GPIO_PORT_RX GPIOA&sharpdefine GPIO_PIN_RX GPIO_Pin_10&s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.