STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MicroXplorer as Eclipse plugin with Linux

Posted on May 31, 2012 at 12:27Hi,does anybody use the MicroXplorer Eclipse plugin with Linux and Eclipse 3.7?Here it either crashes Eclipse or I can't choose an MCU.Moritz #microxplorer-ubuntu64-crashes

Moritz M by Associate II
  • 1873 Views
  • 3 replies
  • 0 kudos

TIM_ICPolarity_BothEdge not available for most timers???

Posted on June 06, 2012 at 07:36Hi. I need to read a digital signal coming into an STM32F100. Timing how long the signal is in a low state and also knowing if the counter overflowed would give me the two pieces of information I need (value of the da...

laurie by Associate II
  • 1998 Views
  • 3 replies
  • 0 kudos

SDIO + DMA + CRC

Posted on September 06, 2012 at 10:49ello,I sometimes have problems with blocks which are written completely wrong onto the sd-card. Workaround: actually I check the written data again by reading the same block from SD-card and check the both buffer...

Problem with two consecutive _SdRead()

Posted on September 03, 2012 at 18:08 Hi, I am using the software example 'MassStorage' , the IAR compiler and the STM32F103ZE kickstart board for development. I wanted to add some functionality which requires consecutives reads from ...

colsman by Associate II
  • 1410 Views
  • 4 replies
  • 0 kudos

STM32F4 not passing EV6 on I2C

Posted on September 06, 2012 at 07:13I'm having some difficulty communicating with a TI INA219 using an STM32F407VE and I2C1 on PB7 and PB8. Sending data seems to work just fine, but receiving it does not. Namely, my EV6 (I2C_EVENT_MASTER_RECEIVER_M...

Help interpreting USB OTG docs for stm32f1xx

Posted on September 05, 2012 at 16:30Hi all! The software design process we use requires that every piece of code is heavily tagged with references to the original programming manuals. Sometimes these tags are added during code reviews, etc. The que...

ashibakov by Associate II
  • 2868 Views
  • 6 replies
  • 0 kudos

STM32F0 - USART1 external clock?

Posted on September 05, 2012 at 03:07Hi!Is there a way to clock (only) USART1 using a (variable) external clock of 1 to 12 Mhz?Also, is there a way to clock USART2 using another clock source than system?Thank you!

Debug without SWD/JTAG

Posted on September 03, 2012 at 09:05Hello everyone,For a project, we try to debug STM32C-Eval board without SWD/JTAG standart board. We have an *.out file and we want to download this file. We want to implement a C/C++ program instead of SWD/JTAG. ...

2 min interrupt using RTC

Posted on September 04, 2012 at 02:47Hi all, I am new to programming. I wanted some help regarding rtc coding. I am using stm32l1 discovery board(and IAR workbench), and want to generate interrupt after every 2 mins. I think using timers for this wi...

STM32F103C6 HSE oscillator Hardfault

Posted on September 04, 2012 at 00:42Hello! Sorry for the new thread I'm new here, and I ran into a strange problem... I have a board with an STM32F103C6 micro, and I'm trying to switch the uC to use the on board  HSE crystal (12MHz) instead of the ...

holcsik2 by Associate II
  • 1812 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.