2012-09-09 7:03 PM
Hello every1,
few days ago i had a problem with uart tx and nw i have solved that problem. so my tx is working fine now. my rx is working too but very slow and gets junk values. below is my code. int main(void) { /* GPIOC clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* USART4 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_UART4);/* UART4_TX */ GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_UART4);/* UART4_RX */ /*-------------------------- GPIO Configuration ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitTypeDef USART_InitStructure; // USART_ClockInitTypeDef USART_ClockInitStruct; /* USARTx configuration ------------------------------------------------------*/ /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - Two Stop Bit - Odd parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; //115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(UART4,&USART_InitStructure); //uart USART_Cmd(UART4, ENABLE); while (1) { if (USART_GetFlagStatus(UART4, USART_FLAG_RXNE) != RESET) { uint16_t x = USART_ReceiveData(UART4); while(USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET); USART_SendData(UART4, x); } } As u can see im trying to loop back whatever data i receive. Im using STM32F4-Discovery board with STM32F407VGT6 IC. any help wud be much appreciated. Vivek #wait-for-you--clive1-!-!-! #wait-for-you--clive1-!-!-! #wait-for-you--clive1-!-!-!2012-09-09 9:40 PM
uint8_t bc;
while{while(USART_GetFlagStatus(UART4, USART_FLAG_RXNE) == RESET); bc = (USART_ReceiveData(UART4) & 0x7F);while (USART_GetFlagStatus(UART4, USART_FLAG_TXE) == RESET);
USART_SendData(UART4, bc);
}
2012-09-09 10:50 PM
thnx vinoth!
i found the problem. it was my interface ic. i was then trying to read a text file(40 KB) using hyperterminal. I can read a part of the file perfectly(say 15-20 lines) and some part is not captured(say 40-50 lines) n so on. my code remains the same as above.2012-09-09 10:51 PM
2012-09-10 6:50 AM
I think, ideally, you want to add some buffering to provide elasticity between the rate the data comes in and the rate it leaves.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.