2012-09-06 11:09 PM
Hi! all,
Is it possible to use i2c of stm32l152rbt6 in a full duplex mode? if so can you post/send me the relevant code for that.thanks, #i2c-in-a-full-duplex-mode #i2c-fundamentals2012-09-06 11:24 PM
Is it possible to use i2c of stm32l152rbt6 in a full duplex mode?
No. The i2c bus has generally no duplex mode. There is just one SDA line. Maybe you mean SPI ?
2012-09-07 6:13 AM
thank you for your reply.
not SPI, i am asking about I2C only. i performed transmission between master and slave ie. master transmitter and slave receiver. now i need to do reverse of it, ie. slave transmitter and master receiver. there is a procedure in stm32l1xx.h(header file) and st's reference manual but i am not understanding that.2012-09-07 7:34 AM
i performed transmission between master and slave ie. master transmitter and slave receiver. now i need to do reverse of it, ie. slave transmitter and master receiver. there is a procedure in stm32l1xx.h(header file) and st's reference manual but i am not understanding that
the usual reason for not understanding the I²C slave to master transfer is thinking ''slave transmitter''. in I²C ONLY the master initiates things read the docs again, but this time think master transmitte and master reader Erik
2012-09-07 7:35 AM
The stm32 can certainly work as master or slave.
But i2c is not spi, there are no separate data connections. The master clocks the bits in or out, but both at the same time, i.e. duplex transmission, is not possible.2012-09-07 1:14 PM
I'm afraid you may not understand how I2C actually works. Please read:
http://i2cbus.com/i2cbasics.html ...and the current I2C spec.2012-09-07 1:55 PM - edited 2024-07-01 3:37 AM
Posted on September 07, 2012 at 22:55
''duplex transmission, is not possible''
To be precise, I2C is half-duplex; full-duplex is not possible.
I2C Specification:
http://www.nxp.com/documents/user_manual/UM10204.pdf
2012-09-08 5:47 AM
To be precise, I2C is half-duplex; full-duplex is
not
possible.Well, I used ''duplex'' as synonym for ''full duplex''. Stating that there are no separate connections (like MISO and MOSI for SPI) should have made it clear. One would assume some interest at the side of the poster to look up for the background, to understand the problem. That well includes the standard paper in this case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.