2012-09-07 12:01 AM
I'm using STM32F0DISCOVERY
I can't receive any char on UART, no interrrupt!Here my initialization:&sharpdefine RCC_PORT_RX RCC_AHBPeriph_GPIOA&sharpdefine GPIO_PORT_RX GPIOA&sharpdefine GPIO_PIN_RX GPIO_Pin_10&sharpdefine GPIO_PIN_SOURCE_RX GPIO_PinSource10&sharpdefine GPIO_AF_RX_PIN GPIO_AF_1&sharpdefine RCC_PORT_UART RCC_APB2Periph_USART1&sharpdefine USART_X USART1&sharpdefine RCC_PORT_DEBUG RCC_AHBPeriph_GPIOC&sharpdefine GPIO_PORT_DEBUG GPIOC&sharpdefine GPIO_PIN_DEBUG GPIO_Pin_8&sharpdefine DEBUG_ON() GPIO_SetBits ( GPIO_PORT_DEBUG, GPIO_PIN_DEBUG )&sharpdefine DEBUG_OFF() GPIO_ResetBits ( GPIO_PORT_DEBUG, GPIO_PIN_DEBUG )unsigned char UART_Init(UART_BPS bps) { NVIC_InitTypeDef NVIC_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable the USART1 Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_Odd; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx; USART_InitStructure.USART_BaudRate = bps; /* Enable GPIO clock */ RCC_AHBPeriphClockCmd(RCC_PORT_RX, ENABLE); /* Enable USART clock */ RCC_APB2PeriphClockCmd(RCC_PORT_UART, ENABLE); /* Connect PXx to USARTx_Rx */ GPIO_PinAFConfig(GPIO_PORT_RX, GPIO_PIN_SOURCE_RX, GPIO_AF_RX_PIN); /* Configure USART Tx as alternate function push-pull */ GPIO_InitStructure.GPIO_Pin = GPIO_PIN_RX; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIO_PORT_RX, &GPIO_InitStructure); /* USART configuration */ USART_Init(USART_X, &USART_InitStructure); /* Enable USART */ USART_Cmd(USART_X, ENABLE); USART_ITConfig(USART_X, USART_IT_RXNE | USART_IT_ERR, ENABLE); BufferTxFree = 1; return 1;}//>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>//ok/** * @brief This function handles USART1 global interrupt request. * @param None * @retval None */void USART1_IRQHandler(void){ DEBUG_ON(); if(USART_GetITStatus(USART_X, USART_IT_RXNE) != RESET) { /* Read one byte from the receive data register */ RxBuf[RxBufWrIdx++] = USART_ReceiveData(USART_X) & 0xFF; if(RxBufWrIdx >= RX_BUF_LEN) { RxBufWrIdx = 0; } CheckBusy(); } if(USART_GetITStatus(USART_X, USART_IT_TXE) != RESET) { BufferTxFree = 1; } DEBUG_OFF();} #stm32f02012-09-07 12:53 AM
I miss something like this in your code:
/* Interrupt at reception */ USART_ITConfig (USART1, USART_IT_RXNE, ENABLE);2012-09-07 1:15 AM
2012-09-07 1:41 AM
It's All OK!!!
In other part of the software I call USART_Cmd(USART_X, DISABLE); and then USART_Cmd(USART_X, ENABLE);But when I disable the UART the configuration of the Interrupt is miss...This Line is NOT CORRECT:USART_ITConfig(USART_X, USART_IT_RXNE | USART_IT_ERR, ENABLE);THIS IS CORRECTUSART_ITConfig(USART_X, USART_IT_RXNE, ENABLE);Thank to ALLWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.