STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

problem with B DMA2_Stream0_IRQHandler

Posted on May 03, 2013 at 00:00Hello ,I still novice in embedded programming and when i use DMA transfer between memories the program is blocked on ''B DMA2_Stream0_IRQHandler'' in the file startup_stm32f4xx.splease it's urgent i need help !!this is...

STM32F40G_eval+linux+eclipse+code sourcey

Posted on April 12, 2013 at 11:41Hi, Am programming my stm32 using eclipse on linux, i configured link resources and i added path, but am having this error: Program ''arm-none-eabi-gcc'' not found in PATH  I don' know why i have this error because ...

STM32F3 discovery SPI communication

Posted on May 04, 2013 at 00:34 hello! i'm an engineering student and i'm workingon a quad-copterproject. i have to use the stm32f3 discovery board to send gyro and accelerometer data throught spi to a rasberry pi board! the first step ...

walpro by Associate
  • 2090 Views
  • 3 replies
  • 0 kudos

EEPROM emulation problem in STM32F0

Posted on May 02, 2013 at 14:13 Hi, I try eeprom emulation but I have problem: I use this function for storage variable: void write_block_eeprom(uint16_t stato,uint8_t *numberbuff){ uint16_t lsb,i; uint16_t checksum; uint8_t msb; ...

the problem of STM32F439 about the LCD_FRAME_BUFFER

Posted on May 03, 2013 at 05:45hello, i have a eval board of STM32F439.i have some problems.the first one:when i used the  LCD-TFT Controller to display the LCD,I found the demo have a code of #define LCD_FRAME_BUFFER   ((uint32_t)0xC0000000)#define...

0690X00000604ydQAA.png
aizhixi by Associate II
  • 1346 Views
  • 2 replies
  • 0 kudos

Clearing the OCxREF signal on an external event

Posted on May 03, 2013 at 11:15HiI'm having a problem with clearing the OC1, 2 and 3 references. I'm using the following code for configuring PE7 as the external trigger and for enabling the OCrefs clear:  /* Configure PE7 as External Trigger Input ...

External SRAM + USART Interrupt IO = USART RX Overrun?

Posted on May 02, 2013 at 15:23I have the following configuration: - STM32F4 MCU - 2 external SRAM chips (at 0x6000000 & 0x64000000) - USART1 running in Interrupt IO mode. - Stack in CCM The SRAM and USART code is almost verbatim from the STM32F4 ...

mfranklin by Associate III
  • 1444 Views
  • 2 replies
  • 0 kudos

get break frame + stm32f103c8t6

Posted on April 25, 2013 at 04:13Hi everyone,I have already had a project about stm32f103c8t6 chip.I used rs485 to transfer data beetwen 2 board via SN751768P IC.I'm sure that all things about schematic are fine.I transfer data without break signal ...

STM32F4 Discovery: ST-LINK bricked

Posted on April 04, 2013 at 14:38Hello, out of a working setup, suddenly I dont get any connection to my ST-LINK anymore And LD1 is blinking red (f ~ 0.5 Hz). PA13/14 are not used in my program. Even in Device-Manager there is no ST-LINK recognized ...

dpfeffer9 by Associate II
  • 2768 Views
  • 6 replies
  • 0 kudos

HELP OMNIVISION CAMERA 0V9655 or OV7675 or OV(anything)

Posted on April 10, 2013 at 14:29Hi.I have the STM32F4DIS-CAM addon board for the STM32F4 Discovery. This addon comes with an OV9655 camera. I also have a OV7675 camera with the same connector and pinout.I am unable to get either of these cameras to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.