STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to debug hard fault handler exceptions?

Posted on March 26, 2013 at 02:34Hey all - thanks for taking your time to helpI have no idea how to track down whats going on. Opening debug explore seems logical - but I have no idea what to do with the address faults. I am not sure what they mean....

Peripheral view while debugging

Posted on May 02, 2013 at 20:52While working through the projects in the STM32F4Discovery Keil examples, the peripherals aren't available for view like they are when creating a standalone project. I can add a watch point for SPI2[as an example] and ...

USART2 problem....

Posted on May 02, 2013 at 19:20i am trying to interface gsm module , I want to use USART2 and USART3 ... but I am not getting how to do that can anyone suggest me ... thank you .. iam attaching the code i am using in the attachments . #rs232-di...

yogee00 by Associate II
  • 4076 Views
  • 7 replies
  • 0 kudos

Audio Compression

Posted on May 02, 2013 at 17:40Does anybody have a good ap note or direction for incorporating software compression on an audio stream? I'm using the discovery board[STM32F4] to record the audio[8KHz 16Bit] and would like to send over a wireless lin...

Audio Playback and Record, DMA from RAM

Posted on April 23, 2013 at 01:28When executing the audio clip from flash[const defined location as in the example project] the audio file plays fine, but if I remove the ''const'' as to allocate ram for the audio clip, I get only a small block of w...

STM32F4 Burned out

Posted on April 18, 2013 at 11:04Hi,I'm using an stm32f4 on a PCB and suddenly it became extremely hot. The strange thing is that it still worked, but there was an extremely (relatively) high current running through the circuit. I've removed the stm...

thommagn by Associate II
  • 3697 Views
  • 6 replies
  • 0 kudos

Adapting SPI from F1 to F0

Posted on April 23, 2013 at 22:41 Hi, I have some working code on STM32F103 that I want to use with a STM32F051 (Discovery board) but I have some troubles to get the SPI communication working. The program get stuck when waiting for an in...

STM32F103 - I2C Slave - Polled works, Int fails

Posted on April 23, 2013 at 12:38 Hi all, Im taking my first steps in trying to get a STM32F103 I2C slave working... Not easy considering what seems to be the complete lack of simple known working examples :( Polling for I2C eve...

mwp by Senior
  • 2132 Views
  • 5 replies
  • 0 kudos

Custom STM32 board bootup problem - Fried MCU? Help!

Posted on April 17, 2013 at 10:11Hi All, I have made a custom board with the STM32F405. When I apply power to the board, the MCU is drawing lots of power (like ~200mA+!). I haven't loaded any code onto it, its straight out of the box. I have 2.2uF c...

generate one pulse

Posted on July 08, 2011 at 06:18I am trying to generate a single pulse using the TIM_SelectOnePulseMode() function in STM32f10x_tim.c source file. But I am not able to get the pulse. why? I am using TIM4 CH2... Any advice? int main(void) {     TIM_C...

kong0073 by Associate II
  • 6336 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.