2013-04-04 5:38 AM
Hello,
out of a working setup, suddenly I dont get any connection to my ST-LINK anymore And LD1 is blinking red (f ~ 0.5 Hz). PA13/14 are not used in my program. Even in Device-Manager there is no ST-LINK recognized anymore. Another Discovery board works perfectly. What can I do to reanimate my precious STM32F4?2013-04-04 7:20 AM
If your code is causing a problem pulling BOOT0 High at start up will remove it from being an issue.
2013-04-04 7:49 AM
thanks for the reply. i tried that, but it didn't work. Maybe the ST-Link Controller is defective?
2013-04-04 7:54 AM
Perhaps, or may be you changed something. Like drivers, or installed something else? Moved some jumpers? Add circuitry, damaged a regulator?
You could try on another system with a fresh install, or try a different discovery on the same system.2013-04-04 11:21 PM
Unfortunately, another identical F4-Discovery works with same setup, jumper-config and USB-cable...
I cannot rule out a surge peak on any pin due to ESD, or that I accidentially touched a pinhead with 5 VDC. Is there any possibility to reflash the ST-LINK part of a discovery board?2013-05-02 8:44 PM
Hi,
Windows 7 does not detect my STM32F0 discovery board. I am getting the following error: Windows has stopped this device because it has reported problems. (Code 43) It was working fine and all of a sudden its not getting detected. Any resolution??2013-05-02 8:45 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.