2013-05-03 2:15 AM
Hi
I'm having a problem with clearing the OC1, 2 and 3 references. I'm using the following code for configuring PE7 as the external trigger and for enabling the OCrefs clear: /* Configure PE7 as External Trigger Input for clearing OCrefs of Timer 1 */ /* and enable OCref Clear for each channel */ RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOE, ENABLE); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_Init(GPIOE, &GPIO_InitStructure); TIM_ETRConfig(TIM1, TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted, 0); TIM_ClearOC1Ref (TIM1, TIM_OCClear_Enable); TIM_ClearOC2Ref (TIM1, TIM_OCClear_Enable); TIM_ClearOC3Ref (TIM1, TIM_OCClear_Enable);Do I have something missing please?I'm using Center-aligned Mode 2 as counter mode and PWM Mode 2 as output compare mode, to control my 3 phase motor. I need to clear the three pwm channel references when PE7 goes high.Thanks in advance,TerenceWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.