2013-04-10 5:29 AM
Hi.
I have theSTM32F4DIS-CAM addon board for the STM32F4 Discovery. This addon comes with an OV9655 camera. I also have a OV7675 camera with the same connector and pinout.
I am unable to get either of these cameras to output anything less than their maximum resolution, so I cannot capture a frame within the RAM of my STM32F407VG.If anybody has managed to do this, could you please let me know what you loaded into the cameras registers, and also what your clock configuration is? I would like an output of 320x240 with RGB565, I don't care about the frame rate or band filtering.The
STM32F4DIS-CAM provides a 24MHz oscillator.
2013-04-11 1:15 AM
I have the BB and the LCD board, but not a CAM board - for exactly this reason.
But there are examples from Embest around, possibly they could help you. As they are rather big, I only have the ethernet, USB, and LCD ones. As said, I never tried anything with this camera extension board, so I can't provide any specific help ...2013-05-02 8:38 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.