STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F207IF use of CAN2

Posted on July 02, 2013 at 18:51 Hi. I am using the KEIL exemple RL-CAN software for MCBSTM32F200 with and board that use stm32f207IF. The problem is that I can't change the pins of CAN2 sucessfully. The CAN works to send a messange but rece...

felipe by Associate II
  • 874 Views
  • 2 replies
  • 0 kudos

STM32F4xx IAP - passing arguments

Posted on July 12, 2013 at 00:17Hi, I'd like to have algorithm executing application (from 0x8004000) operating on data buffered in my modified IAP firmware (2 x (uint16_t [128]) located after IAP code, before 0x8004000). But after compiling my IAP ...

identify the PORT generating an EXTI

Posted on July 14, 2013 at 15:10dear all,   I hope this finds you well. I am relatively new to such technology and I am working on some drivers. The board I am using has 4 LEDs, a joystick and a couple of buttons (WAKEUP and USER). I have implemente...

F4 Flash Write - random or sequential?

Posted on July 11, 2013 at 15:19 Hello, is F4 Flash write can be random or only sequential? I've tryed to do FLASH_Unlock(); FLASH_EraseSector(FLASH_Sector_8, VoltageRange_3); for(i=0, EEAddr=EEA;i<32;i++){ FLASH_ProgramWo...

printf with 2's compliment

Posted on July 13, 2013 at 08:46I ported the printf functions to UART3. I am reading some gyro data from a digital chip that gives it's results in 2's compliment. So I get the raw data and print the integer that I stored it in. But the printf functi...

STM32F303 Discovery board ADC offset

Posted on June 13, 2013 at 09:18Hi, I've configured ADC1 to sample one of the channels like PA1 (Channel 2). However, when I connect a power supply to the input, there is a large offset. For example, connecting 2V I can see around 200-250mV offset. ...

gustavo by Associate
  • 2090 Views
  • 5 replies
  • 0 kudos

STM32F3 Discovery - ADC Offset

Posted on July 10, 2013 at 23:04I'm working on getting the ADC fully integrated with the rest of my code.  When I'm testing out my ADC, however, I keep getting an output of about 300-400 from ADC1->DR when I'm inputting a voltage of 0 to the pin.  I...

mattfox by Associate II
  • 2131 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.