2013-06-13 12:18 AM
Hi,
I've configured ADC1 to sample one of the channels like PA1 (Channel 2). However, when I connect a power supply to the input, there is a large offset. For example, connecting 2V I can see around 200-250mV offset. Below is my code. I can see the adc value change with the change in input voltage, but I am not sure whether some specific calibration is required. Any insight is appreciated. GPIO_TypeDef * adcChanPortType; ADC_InitTypeDef ADC_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure; /* Configure the ADC clock */ RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2); /* Enable ADC1/2 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); /* ADC Channel configuration */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(adcChanPortType, &GPIO_InitStructure); ADC_StructInit(&ADC_InitStructure); /* Calibration procedure */ ADC_VoltageRegulatorCmd(ADC1, ENABLE); // Insert delay equal to 10 µs // To allow regulator to settle unsigned long int i = 4800; for(;i>0;i--); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1) != RESET ); //calibration_value = ADC_GetCalibrationValue(ADC1); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0; ADC_CommonInit(ADC1, &ADC_CommonInitStructure); ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable; ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0; ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); /* ADC1 configuration */ ADC_RegularChannelConfig(ADC1, adcChanNum, 1, ADC_SampleTime_181Cycles5);2013-06-13 6:36 AM
Disconnect the power supply and connect board ground to PA1 to see if is a grounding problem with the power supply.
Cheers, Hal2013-06-13 8:23 PM
Hal,
I did so. When I connect ground I see 0 at the output. When the pin is floating I see 160/170mV. Thanks2013-06-14 5:23 AM
That is normal. The sample and hold channel capacitor will drift if the input is not connected to a low impedance signal.
You didn't say, but I am guessing the power supply signal source is grounded to the wall socket, and so is the Programming/debug PC providing ground to the board. Or you have something similar causing a ground loop. You are using a long sample time, so the problem is external to the processor. Cheers, Hal2013-07-12 12:19 PM
Hi,
I've been having a really similar issue as you, where I have my ADC running really well except for when I have USART connected (or any driven pin for certain pins around the ADC). I described my problem here: [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F3%20Discovery%20-%20ADC%20Offset&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx¤tviews=25]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32Discovery%2fSTM32F3%20Discovery%20-%20ADC%20Offset&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FAllItems%2Easpx¤tviews=25I was wondering if you made any progress or learned a solution to this problem, as I can't seem to find one anywhere online. I'd love to hear about how you've moved forward with this problem!2013-07-12 8:06 PM
I figured out the solution just now. If anyone is interested, I posted a fairly detailed solution on the thread that I linked to above.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.