STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 discovery - Recieve ''char or word '' from RX.

Posted on July 02, 2013 at 06:08i have a problem with recieve data to stm32. send data to UART works fine in hyperterminal on windows i see all wordl who send stm32. But we need to STM32 could also receive data from the computer.I need to able to re...

polasek by Associate II
  • 3448 Views
  • 7 replies
  • 0 kudos

USART RX interrupt - capturing data

Posted on July 12, 2013 at 09:46Hi all,I am working USART RX interrupt.I am sending command through rs485 interface (usart TX) and waiting(delay) response from external device.What i wonder is , there is a flag for waiting last received data?i dont ...

Embedded SRAM as the boot space

Posted on July 12, 2013 at 09:52In AN2606 it's described when both BOOT0 and BOOT1 are pulled-up, Embedded SRAM is selected as the boot space. How can I load my application to SRAM without programming FLASH and run it after loading without any reset...

rahmani by Associate
  • 1179 Views
  • 1 replies
  • 0 kudos

f4 discovery rs232 baud problem

Posted on July 11, 2013 at 10:29Hi, I have it working but seem to get about 1/3 of the baud rate that I program into USART_InitStructure.USART_BaudRateIn other words, I have to set it to 9600*3 to get a baud rate of approximately 9600 baud.Maybe I h...

ian239955 by Associate II
  • 1807 Views
  • 4 replies
  • 0 kudos

STtub driver under windows 8

Posted on July 04, 2013 at 12:39I'm trying to get DfuSe application working under windows 8, but I have problem with installing the STtub driver for device in dfu mode. I have tried to install it with disabled forcing of signed driver in win 8, but ...

pa2 by Associate II
  • 2653 Views
  • 5 replies
  • 0 kudos

STM32F407 ADC Scan operation

Posted on July 11, 2013 at 16:17The STM32F407 ADC(s) support scan mode where a predetermined group of ADC input channels are successively converted with the results DMA'd to a circular memory array at the end of the group conversion. This works but,...

John F. by Senior
  • 590 Views
  • 0 replies
  • 0 kudos

STM32F4Discovery RTC+VBAT reset

Posted on July 10, 2013 at 16:33Hy all! I've a STM32F4Discovery board. I want to use the RTC library. I see the board schematic, and I think the VBAT pin is always on VDD. I configure the RTC with LSI, and wake up event, and write a number to the b...

totti001 by Associate II
  • 2161 Views
  • 5 replies
  • 0 kudos

STM32F2 JTAG without NJTRST unusable

Posted on June 30, 2013 at 00:29We have a STM32F205RCT6 connected via JTAG. The JTAG emulator uses TDI, TDO, TMS, TCK and SRST (system reset). The NJTRST (JTAG reset) pin is electrically not connected to the JTAG pin header. As long as the softwar...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.