2013-01-21 10:48 AM
I have a STM32-F4 discovery board, specific model ♯ STM32F407 VGT6. Having connected it to my computer via USB I have successfully run its test programs. Additionally I have successfully built a test program that came with IAR EWARM 6.5.
However, I notice that IAR, the ST Link Utility, etc. have been unable to download programs to the board. I noticed that the Devices & Printers section of the Control Panel recognizes my board but has a yellow icon under the device icon, with status ''needs troubleshooting'' and ''driver is unavailable'', despite having installed the USB driver and the STLINK driver showing up in the programs & features section of control panel. (On edit) Eventually I got my board to work on my old computer that had windows 7. #stm32-f4-discovery2013-01-21 12:10 PM
Windows 8 won't load unsigned drivers without intervention
2013-01-21 4:57 PM
Already tried that twice, re installing driver under non enforcement mode, but the troubleshooting wizard from Devices & Printers still can't find the driver. Should I copy the STLinkUSBDriver.dll file to that Drivers folder in C:\Windows\system32 or someplace?
2013-01-21 5:57 PM
I'm using Keil 4.60, not IAR, but this did work for my Windows 8 install which up to that point wasn't working.
C:\Keil\ARM\STLink\USBDriver\ST-Link_V2_USBdriver.exe (3-21-12 8:59:18) You might want to check if you have the most current firmware on the ST-LINK. I don't think the system is going to entertain copying files into critical directories.2013-01-21 7:18 PM
Upgraded the firmware, even dl'ed Keil 4.6, still no luck. Up to now I've never had USB issues with my computer, which I got for christmas and had win8 pre-installed.
2013-07-15 4:13 AM
1) Type devmgmt.msc in Search bar
2) Click onDevice Manager
3) on other device Click stm32 discovery for unlock and install device that could be work.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.