STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDIO Libraty for STM32F417 or programming manual for CooCox

Posted on June 13, 2013 at 16:04Hi everyone!Could you give me a complete example for SDIO raw read/write with 4-bits wide bus and DMA?I'm trying to do it in Coocox CoIDE. Unfortunately there are no examples included. Could you write a manual step-by...

M_1 by Associate II
  • 2903 Views
  • 6 replies
  • 0 kudos

Position independent code on STM32F2xx

Posted on July 17, 2013 at 13:24I'm trying to create a position-independent application that will run in one of two possible locations in flash as part of a firmware update process. A 'live' application will download a new application, check it for ...

richard by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

USART

Posted on July 17, 2013 at 05:19 I tried configuring. Im using the STM32F103RB /* Setup GPIO pin GPIO_USART1_TX. */ GPIO_InitTypeDef GPIO_InitStructure; // GPIO structure USART_InitTypeDef USART_InitStructure; // USART Structure USART_ClockIn...

timothy by Associate II
  • 1470 Views
  • 2 replies
  • 0 kudos

DMA timer capture

Posted on July 16, 2013 at 16:42Hi,I need to do some timming analyses on signal. I use the capture mode of a timer.When I use the interrupt to capture event, it works but when the signal is fatser I get into overrun issue, I cannot run my CPU faster...

Adalgiso by Associate II
  • 1595 Views
  • 2 replies
  • 0 kudos

Send data with usart in smart card mode and DMA

Posted on July 16, 2013 at 00:26Hi, I'm trying to communicate with a smart card using the usart on a STM105RC. I was successful doing that with normal interrupts, and now I'm trying to use the DMA with the USART for better performance. My problem is...

STM32F405 Custom Software Triggered Interrupt

Posted on July 16, 2013 at 12:39Hi,I was wondering if it is possible to define software triggerd interrupts, i.e. an ISR is triggered by a value change of an arbitrary register.Any help is appreciated! #stm32f4

ole by Associate
  • 1364 Views
  • 2 replies
  • 0 kudos

Timer/Pwm

Posted on July 15, 2013 at 15:03 Hi, I'm working with STM3220G. I have to create a project that: configure GPIOA(pin1) in output for 20msec. After 20msec, starts a PWM for 5msecand so on... My problem is: when I see in myosciloscope, the wave...

0690X00000604zRQAQ.png
mosine by Associate II
  • 1874 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.