STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

inconsistent Calibrations values.

Hi.. Can anyone tell me why the ADC Calibration value is not the same before and after I initialize the DACIt seems that the value maxes out if I calibrate after I have initialized the DAC.The calibration register is 7 bits.The ADC also measures inco...

DAC_ADC.jpg
spa23 by Associate III
  • 2393 Views
  • 4 replies
  • 0 kudos

Resolved! Reading data with BRS on fdcan line

  I am using STM32H5RE23T6. I implemented the function of receiving data from the FDCAN line. When I select FDCAN mode without BRS, it works without any problems. When I select with BRS mode.I set the arbitration phase to 1mbps.I set the data phase t...

CANZT-FD by Associate III
  • 3211 Views
  • 6 replies
  • 1 kudos

Resolved! USART used as GPIO to send break signal for DMX-512

Hello!I am just getting started with STM32 universe. I've already finished my first project using the IDE SW4STM32 and I board I've designed using the STM32F070CBT. I've also used STM32CubeMX to generate the basic code.I wanted to keep using this boa...

Resolved! Parallel TFT Display not working

Hello Guys, Currently I am using Parallel RGB888 TFT display with resolution 800X480 in which I am using STM32F429ZIT6 controller using LTDC with DMA2 and I am printing whole RED color on display but display showing lines. My question is as I am not ...

Resolved! About the negative ref voltage supply to STM32H753ZI

Hi,    The datasheets says (P173) - the VREF– s available only on UFBGA176+25 andTFBGA240+25. When VREF- is not available, it is internally connected to VDDA and VSSA. Our ADC input signal goes to both positive and negative. Questions:1. What the par...

Output comparison pulse problem

On the stm32h750, I want to use 4 channels to implement pwm waves with different phases in the output comparison mode of tim8. Chanel's mode selection switches on match. The stages are 0% 25% 50% 75%. When the phase is zero (sConfigOC.Pulse = 1-1), t...

S__101253122.jpg
hao by Associate
  • 1659 Views
  • 3 replies
  • 0 kudos

STM32 REMOTE DEBUG

Hello,I have designed several custom boards based on STM32 MCUs, And are running fine problem is i have installed these across the country over 50 locations and now it very costly to go to each location for for required software updates or to debug i...

psain.1 by Associate III
  • 5364 Views
  • 10 replies
  • 2 kudos

What is up with STM32H563 ADC INP0?

Hi,I am not able to get a correct reading from ADC1 INP0 (PA0). All the other analog channels works fine.The datasheet mentions this:ADC option register (ADC_OR), option bit 0 (OP0)For ADC1:0: INP0/INN1 GPIO switch control disabled1: INP0/INN1 GPIO s...

Dimlite by Associate III
  • 4075 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.