Stm32F303 Jump to app not working
hello.After Mcu jump to app in custom bootloader, work while(1).Jump code is not working.
Ask questions, find answers, and share insights on STM32 products and their technical features.
hello.After Mcu jump to app in custom bootloader, work while(1).Jump code is not working.
Hi!I'm working on a product that requires a very fast response time for capacitive touch sensing (in the order of <5ms). I'm currently looking into the TSC module in some STM32 controllers. However, I can't seem to find any information regarding the ...
I am working on a project where the end goal is that TIM8 is used to capture an incoming PWM signal on PC6. I want TIM2 to trigger from TIM8 and generate a single pulse on PB11. I have TIM8 working, capturing both rising and falling edges properly. ...
I doing bare metal coding for STM32L496ZGT6. Now in SPI, extra bytes are sent. There are only 4 Registers in SPI but unable to resolve the issue. Below is my codeNOTE:I am using Aardwark Total Phase Control Center software for debugging. I am attachi...
Board: STM32 Nucleo-F411REI am trying to get audio from I2S MEMS microphone (SPH0645). According to datasheet here - https://www.knowles.com/docs/default-source/default-document-library/sph0645lm4h-1-datasheet.pdf Basically I am supposed to get a 32-...
I haven't been able to wait 500ms without affecting the timers for 7 days.In this block, doesn't PB14 become "0" after 500ms?Even if I use comment lines, it doesn't work.Note: volatile uint32_t Counter = 0;The "Counter" variable is incremented every ...
Hello ST Team,I am working on a project in which I want to interface NucleoF446RE board with 2.4inch LCD Display Module,240x320 Resolution, SPI Interface. I have already implemented code for SPI interface and using readymade ILI9341 library I have te...
Hi !I got some samples of G473CBTx from ST through one of the official distributor, which were populated on prototype boards. I am trying to flash them, but unfortunately stumbled upon the "no STM32 Target found" error. I tried the following. 1. Use ...
"In the STM32U5, the LPTimer is used to periodically wake up from Stop 2 mode to sample ADC data. After the ADC samples the data via DMA and generates an interrupt, the system re-enters Stop 2 mode. When using a debugger, the sampled data is normal. ...
hello what is the diffrence between stm32f29i-disc1 and stm32f429zi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.