STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! One by one port pin configuration locking

There is no clear information in the reference manual about port pin configuration locking one by one. For example (desired code): void SomeFunction() { // locking pin configuration one by one LL_GPIO_LockPin(GPIOA, LL_GPIO_PIN_0); LL_GPIO_Lock...

brat0x2 by Associate
  • 2122 Views
  • 4 replies
  • 3 kudos

STM32U5 - does OctoSPI support inter-byte spacing?

Hi there,I'm working on a project with the STM32U5. This MCU comes with both a SPI and a OCTOSPI peripheral.The SPI peripheral supports a setting called MasterInterDataIdleness - in the reference manual it's shown as "master Inter-Data Idleness", whi...

nethecite by Associate III
  • 3332 Views
  • 7 replies
  • 0 kudos

Resolved! LPTIM Multiple odd behaviours

I am writing an LPTIM driver without HAL or LL drivers on the B-L072Z-LRWAN1 board. I have been getting a number of odd behaviours here that I am hoping someone here can shed some light on.1) cannot enable continuous start          -bit 2 of the CR r...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.