2024-11-21 4:30 AM
Hi STM32 Team,
I am working on implementing a USB Mass Storage Class (MSC) application on the Nucleo-F439ZI development board. My objective is to use the Fat Fs file system to read/write data from/to a USB flash drive.
I need example code for that. For example I need to create a text document.
Kindly do needful,
Thanks and Regards,
A. Ajith Kumar
2024-11-21 7:59 AM
Hi @ajith1
Check the following example
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.