2024-11-21 9:36 AM - last edited on 2024-11-21 9:47 AM by Andrew Neil
Issue with SPI DMA Transmission Starting from Random Index Instead of Array Start (Circular Mode) (STM32L562VET6)
I am working with an STM32L562VET6 and have a 2D array DATA defined as follows:
uint8_t DATA[NOS][3] = {};
Here, NOS = 20000, and each row of this array contains a 24-bit integer value split into three bytes. For example:
DATA[3][0] = 0x00;
DATA[3][1] = 0x00;
DATA[3][2] = 0x03;
I’m transmitting this array using SPI with DMA in circular mode, like this:
HAL_SPI_Transmit_DMA(&hspi2, DATA, (uint16_t)(NOS * 3));
On the receiving side, I merge the three bytes back into a 24-bit integer. However, instead of the values starting from 0 (from DATA[0][0]), the transmission starts from some random index, goes up to 19999, and then wraps around to start again from 0 to the random starting index.
Why is the transmission not starting from DATA[0][0] in circular mode?
How can I ensure that the transmission always starts correctly from the beginning of the array?
Any insights or suggestions would be greatly appreciated! Thank you so much in advance!
2024-11-21 1:25 PM
And what's the code for the receiving party? How do you ensure the the reception starts in sync with transmit?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.