STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TIM1 update does not request DMA

Hello,I'm trying to generate a custom PWM output signal with the F103V8TxLQFP100. I took inspiration from here: Custom Signal generation using PWM and DMA - STMicroelectronics CommunityThe basic code looks like this:...uint8_t tempBuffer[10];tempBuff...

DP_42 by Associate II
  • 2066 Views
  • 2 replies
  • 0 kudos

Resolved! Dual bank flash organization on STM32U5

I've been looking at the information on the flash organization in the Reference manual RM0456 for STM32U5.  In particular I'm trying to understand how the DUALBANK flag works on this family.In section 7.3.1, there is this table for STM32U5G with 4MB ...

williamsone_0-1732607763642.png

Resolved! Unable to activate LWIP on STM32H757IIT6

I am not able to activate LWIP middleware for M7 core on any dualcore STM32. (I am able to do it on single-core devices and  already have LWIP working on H743 Nucleo)Steps I have done (exactly in this order):- create a new project for STM32H757IITx i...

STM32G431 PLL settings to get 170MHz

I have been working on a self learning project with STM32G431 controller. I am having trouble switching on the PLL to get 170MHz.When I use the CubeIDE, I get the 170MHz clock. Given below is my code on how I am trying to Initialize the PLL//PLL sett...

SingularEngineer_0-1732599989122.png

I2C Digital Filter use case

Hello Community, I am planning to use I2C operating at 1kHz maximum on STM32G4 & STM32G0 series for measuring temperature from Digital Temperature sensors placed at 2m distance from the main board in an industrial environment using CAT6 (STP) Cables ...

Chubs by Senior
  • 3696 Views
  • 1 replies
  • 0 kudos

Internal Timer of STM32F767

Hello All, I am using the Internal RTC of STM32F767 MCU. The VBAT pin is connected to an External 3.3V Coin Cell Battery At Power ON (Debug window on STM32 Cube IDE), before HAL_INIT when i see the value of RTC BKP1R Register it is 0x5432 as I intend...

akash_praan_0-1732636383756.png akash_praan_1-1732636408137.png

STM32G431 SPI Strange Data

Hi Everbody,im trying to setup a SPI com with a DRV8301. im using de STM32G431CBU6. a have read the datasheets mutiple times not saying that i did everything correct but i dont see it anymore. i was hoping that its just a *** mistake and some can pin...

Ruben_Konings_0-1732620705369.png Ruben_Konings_1-1732620740215.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.