STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750B-DK Debug issue with SCB_EnableDCache

Hi all. I am aware that this topic has been discussed before here:  https://community.st.com/t5/stm32-mcus-products/debugger-hangs-at-scb-enabledcache/td-p/640648 and here: https://community.st.com/t5/stm32-mcus/dma-is-not-working-on-stm32h7-devices/...

Dual ADC mode single DMA configuration - How?

The STM32H7(4/5) documentation states that two of the ADCs on board can be used in dual ADC mode, so that their 16bit samples are read into the upper- and lower halfwords of a single 32bit register (ADCx_CDR), from where a single DMA can read them in...

MHilt.1 by Associate
  • 5476 Views
  • 5 replies
  • 1 kudos

Resolved! Is bank swap of stm32h523VCT6 possible?

I checked the datasheet and there is a memory map of 521Kbyte.But I use the stm32h523VCT6 chip.This chip has 256Kbyte of memory.Can't a chip with 256Kbyte of memory use bankswap?If it can, can you tell me the memory address? 

Roy_Lee_0-1732553972220.png
Roy_Lee by Associate
  • 1104 Views
  • 2 replies
  • 2 kudos

Resolved! Initial project using STM32H745BIT3 supporting FDCAN

Hi: I'm a "newbie" to STM processors. I have a board with the STM32H745BIT3 processor on it. I'd like to get the board to initially communicate via FDCAN to my laptop. My laptop has a PEAK FDCAN device on it. Is there a base CubeIDE project or .ioc f...

KennyD by Associate
  • 1690 Views
  • 3 replies
  • 0 kudos

STM32H7 - USB High Speed - External Phy

I'm using an STM32H750 MCU to run an application that communicates with a computer via USB in CDC ACM mode. The application uses USBX from Eclipse ThreadX and an external USB PHY (USB3300) to perform high-speed communication. My application works fin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.