STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F042 SWD comunication Problem

Posted on November 23, 2014 at 19:08I have designed a board with a microcontroller STM32F042K where SWD does not work. I connected pin 4 (NRST) with a pull-up 100Kohm and a 100nF capacitor to GND and pin (BOOT0) to GND with a resistance of 470ohm bu...

elb-lab by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

CubeMX project generation problem

Posted on December 01, 2014 at 18:18I want to generate TrueSTUDIO projects with CubeMX (4.5.0), because that project format fits my needs (arm-gcc, suitable startup code and linker script). However, I get an error message at the end of the code gene...

redecker by Associate II
  • 1855 Views
  • 3 replies
  • 0 kudos

STM32F4 Discovery change timer ARR on the fly

Posted on December 10, 2014 at 18:41Hello everyone!I am experiencing problem with my discovery board. I am trying to accelerate my stepper motor, so when i push the button, i decrease value in TIM2 ARR with this command:uSeconds-=20;TIM_SetAutoreloa...

anze2 by Associate II
  • 3638 Views
  • 5 replies
  • 0 kudos

ST32f407vgt6 sdcard fatfs problem

Posted on December 01, 2014 at 22:45STM32F4CUBEMX 4.5.0FIRmware 1.3.0in the mode  hsd.Init.BusWide = SDIO_BUS_WIDE_1B; everything works well but in mode   hsd.Init.BusWide = SDIO_BUS_WIDE_4B;retSD = FATFS_LinkDriver(&SD_Driver, SD_Path);    -  RES_O...

STM32 CUBE SDIO 4bit problem

Posted on November 24, 2014 at 16:19Hello;I want to use 4Bit SDIO on STM32F407VGT6 MCU. I already set all parameters on lastest STM32CubeMx software. RCC => External XtallSDIO =>4bit busMy Ide is KEIL 4.73.But this configuration is not working. When...

emre by Associate II
  • 1327 Views
  • 1 replies
  • 0 kudos

I2C interrupt driven communication problem!

Posted on December 11, 2014 at 14:18Hello friends! I'm using I2C1 on a STM32F103CB, according to AN2824 and reference manual. My goal is to use I2C with lower priority interrupts. For that purpose, i dont use ITBUF, but only ITEVT interrupt. The i2c...

atakan by Associate II
  • 965 Views
  • 0 replies
  • 0 kudos

STM32F103 Standby Mode Resets Processor Immediately

Posted on December 11, 2014 at 10:04Hello,I'm trying to use the STANDBY low power mode on the STM32F103. I have verified that the User Option Bits are set such that IWDG=1, NoReset_STOP=1, NoReset_STBY=1. Therefore the processor should not reset whe...

brent23 by Associate
  • 966 Views
  • 0 replies
  • 1 kudos

Looking for a useful debugger, such as GDB

Posted on December 02, 2014 at 01:32Hello,Recently my team and I have run into a lot of issues in our code that require a good debugging solution. Unfortunately, however, we haven't found a good way of setting breakpoints and stepping through our co...

matt2399 by Associate II
  • 2284 Views
  • 4 replies
  • 0 kudos

STM32F10x SPI DMA sync problem

Posted on October 28, 2014 at 12:16I use two STM32F103R8 controllers that will communicate full duplex SPI with DMA, transmitting 50 integers from master to slave and vice verse. I can't get the data synchronized properly. It seems that the slave is...

bob by Associate II
  • 2457 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.