2014-12-01 9:18 AM
I want to generate TrueSTUDIO projects with CubeMX (4.5.0), because that project format fits my needs (arm-gcc, suitable startup code and linker script). However, I get an error message at the end of the code generation process:
''The Code is successfully generated under <PathToMyProject> but TrueSTUDIO 4.3.1project generation have a problem.'' The generated code includes all headers and source files as expected, but no linker script and no TrueSTUDIO project file. What can be the reason for this error?2014-12-08 1:05 AM
After looking at the output when starting from command line, the last exception pretty clearly points out what's wrong:
java.net.MalformedURLException: no protocol: /home/username/builds/STM32CubeMxInstall/db/plugins/projectmanager\devices\stm32boards.db
at java.net.URL.<init>(URL.java:586) at java.net.URL.<init>(URL.java:483) at java.net.URL.<init>(URL.java:432) at com.sun.org.apache.xerces.internal.impl.XMLEntityManager.setupCurrentEntity(XMLEntityManager.java:619) at com.sun.org.apache.xerces.internal.impl.XMLVersionDetector.determineDocVersion(XMLVersionDetector.java:189) at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(XML11Configuration.java:812) at com.sun.org.apache.xerces.internal.parsers.XML11Configuration.parse(XML11Configuration.java:777) at com.sun.org.apache.xerces.internal.parsers.XMLParser.parse(XMLParser.java:141) at com.sun.org.apache.xerces.internal.parsers.DOMParser.parse(DOMParser.java:181) at stm32Families.Families.getStartupFile(Families.java:94) at convertor.Convertor.getStartUp(Convertor.java:156) at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.getStartUp(ToolchainGenerator.java:99) at com.st.microxplorer.plugins.projectmanager.model.ConfigFileManager.writeUsedFiles(ConfigFileManager.java:497) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:359) at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:36) So CubeMX is trying to access a path with backslashes:<InstallationDirectory>/db/plugins/projectmanager\devices\stm32boards.db
which doesn't work on the virtual windows machine I'm using it on. It also doesn't work on linux (it's a java application after all so I just tried it on ubuntu 14.04. It runs, but can't generate the project)2014-12-11 7:05 AM
Please use the following workaround: in TrueStudio, open the ''Properties'' interface and verify the compilation settings, then press ''Apply''.
Best regards2014-12-11 8:39 AM
Do I need to have TrueStudio installed for CubeMX to work correctly? As I understand it, your reply implies that I would have to load something in TrueStudio before I can apply any compilation settings.
In fact, I don't have or use any of the officially supported development environments. I select TrueStudio output in order to have a working set of source and header files for use with arm-gcc, which is (afaik) the toolchain behind TrueStudio. The files that *are* generated by CubeMX before the error message is emitted include all necessary files, but the linker script is missing. The TrueStudio project file is missing as well, but I don't need it.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.