2014-11-23 10:08 AM
I have designed
a board with
a microcontroller
STM32F042K
where
SWD
does not work
.I connected
pin 4
(
NRST)with
a pull
-up100Kohm
and
a
100nF
capacitor
to GND
and pin
(
BOOT0)to GND
with a resistance of
470ohm
but
ST
-LinkUtility
says
can not connect
with the
target
.
I tried with
a
STM32F051K
and
SWD
works well
.Can anyone help me
?Thanks
!I've #stm32f042-swd2014-12-11 8:40 AM
Hello!
You do not need a pull up resister with this part. It is built-in and enabled by default. I use a larger cap (10uF) because I have a bunch of them and that works for me. When I've gotten errors with SWD not working, I hadn't powered all the power pins (1,5, 17) DanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.