STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Slave is giving garbage values.

Posted on December 10, 2014 at 19:15I have configured my STM32F407 Discovery Board as slave with a STM8S00. The data sent by Master on MOSI is totally different from that which that my slave is receiving I have observed that data on the Digital Osci...

ADC initialization error. USART conflict?

Posted on December 10, 2014 at 23:04 Hello, I'm trying to initialize my ADC to continuously sample, but I must have overlooked something since I'm stuck when waiting for ADC_FLAG_ADONS. I'm programming to the STM32L152C Discovery boa...

sawtooth

Posted on December 10, 2014 at 17:26how i can generate a wave sawtooth ? please i need somone help me  #poorly-framed-question

Relocate app in STM32F105

Posted on December 01, 2014 at 21:36Hi!On a board with a STM32F105 uC I am implementing a uSD bootloader. First of all I wanted to relocate the application to a different address in flash, but I'm getting a stack pointer error.Here the 2 changes:Lin...

gabriele by Associate II
  • 2672 Views
  • 6 replies
  • 0 kudos

ADC3 DMA problem

Posted on December 10, 2014 at 07:30 I am using DMA2 for ADC3 Channel 13,Continuous conversion. #define ADC3_Buffer_Storage_Address ((u32)0x40013C4C) DMA_Struct_Object.DMA_PeripheralBaseAddr=(u32)ADC3_Buffer_Storage_Address;//ADC3 Address...

balu by Associate
  • 1036 Views
  • 1 replies
  • 0 kudos

STM32F4 PWM

Posted on December 05, 2014 at 19:08Hello, I'm trying to change the  duty cycle of TIM1 in PWM Mode, but somehow my code is not working. void TIM1_CC_IRQHandler(void) {   HAL_NVIC_ClearPendingIRQ(TIM1_CC_IRQn);   HAL_TIM_IRQHandler(&htim1);     cx++...

lk1991 by Associate II
  • 1450 Views
  • 2 replies
  • 0 kudos

DMA problem is using ADC1 scan mode

Posted on December 04, 2014 at 21:30hello guysI am using stm32f103RETI want to use ADC1 in scan modeI do software start conversion in a timer interrupt and I configured DMA to save conversion values to a memory buffermy configuration code is herevoi...

abbas by Associate II
  • 1169 Views
  • 3 replies
  • 0 kudos

One pulse generator on STM32L052

Posted on December 05, 2014 at 13:46Hi family,I am trying to generate a determined width pulse in one GPIO pin with STM32L052C uC and I am thinking to do this with One pulse mode timer.Is it possible to do that?Detecting the pulse Tp with the timer2...

0690X00000602z5QAA.jpg
gerardo by Associate II
  • 3527 Views
  • 8 replies
  • 0 kudos

strange problem with keil uvision 5 and interrupts

Posted on December 06, 2014 at 23:52hello , first of all sorry for my bad english. I have problem with isr on keil uvision 5. Simple exception handler, for instance handler for systick interrupt defined as: void SysTick_Handler(){   ....code... } do...

andjelko by Associate II
  • 3547 Views
  • 6 replies
  • 0 kudos

STM32F439 and external core supply: NOT WORKING!

Posted on December 09, 2014 at 20:10 BYPASS_REG = High, VCAP = 1.2V (supplied externally), VCC = 1.8...3VResult: NRST is driven low constantlyby the MCU, nothing works. The same board works OK when BYPASS_REG = Low and the core's external supply dis...

our by Associate II
  • 2459 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.