STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 RTC Time lags

Posted on November 24, 2014 at 15:13Hi,I'm using STM32l151rbt6 MCU. But after few days of running the program the internal RTC starts lagging. I'm not doing RTC calibration. Any other possible reasons?Thanks. #stm32 #rtc

Pending TIM bits

Posted on December 12, 2014 at 08:57Hello forum, I have a weird issue with TIM's pending bits (I mean Cortex-M3 pending bits): they are set after enabling the overflow interrupt: void InitTIM4() {   TIM_TimeBaseInitTypeDef timer;   TIM_TimeBaseStruc...

SPI DMA recover from data shift

Posted on December 11, 2014 at 16:26The original post was too long to process during our migration. Please click on the attachment to read the original post.

bob by Associate II
  • 2084 Views
  • 4 replies
  • 0 kudos

STM32F0 - SPI 8bit data size

Posted on December 12, 2014 at 08:53I am migrating code from STM3210x to STM32F0xx. major part of the application uses spi interface. I see in logic analyzer each bursts of 16bit clocks. while I expect it to be 8bit clock for each byte and a delay o...

roy23 by Associate II
  • 1184 Views
  • 0 replies
  • 0 kudos

STM32CubeMX is nice! Where are the examples?

Posted on December 12, 2014 at 02:58Hi there,   STM32CubeMX looks like it will be quite nice.  Where are the example files?I don't see any example files anywhere.I'd love to see examples of:* basic gpio interrupt usage* DMA to/from I2S/serial port (...

caleb by Associate III
  • 1304 Views
  • 3 replies
  • 0 kudos

Frequency Capture Issue - missing pulses

Posted on December 11, 2014 at 03:32 Hi, I ma currently trying to use the timer capture to measure a burst pulse but it always seems to miss a couple of signals. I have measured it on an oscilloscope and I can see 10 pulses but from my f...

paul23 by Associate II
  • 2339 Views
  • 8 replies
  • 0 kudos

STM32F1 I2C Stops on Slave Pull Down

Posted on December 12, 2014 at 02:46 Hello, I'm having an odd issue with the I2C peripheral. I have a simple routine for writing a value to a slave device register below. It succeeds writing to the slave as seen in Image #1. Following tha...

k3nt00 by Associate II
  • 736 Views
  • 0 replies
  • 0 kudos

LCD TFT Controller (LTDC) frame rate .

Posted on December 11, 2014 at 13:09Hullo guys , I was wondering about the frame rate of the LTDC in STM32F4xx series , There is no obvious information in the user manual about the frame rate , and in the demo example , I just set the pixel value in...

STMPE811 touch controller on STM3220G-EVAL - bug?

Posted on December 11, 2014 at 18:13I noticed that the touch controller is not working properly to detect presses of the touchscreen on the STM3220G-EVAL and looked further into the code.  The problem appears to be rooted in BSP_TS_GetState() in the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.