STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC with DMA arrest on STM32F4

Posted on December 09, 2014 at 14:19Dear All,My board is 429I-DISCO. I tried to code a continuous A/D conversion via DMA on FreeRTOS. At first A/D conversion shortly after power-up was starting nomally by ADC_SoftwareStartConv(ADC3). On the rest of ...

yoshi by Associate II
  • 3966 Views
  • 11 replies
  • 0 kudos

ARM Accredited MCU Enginner

Posted on January 08, 2015 at 07:09A Question and Answer Book ''ARM Accredited MCU Enginner''http://www.amazon.com/dp/B00R9BYWWA #arm-cortex-accredited-mcu-aame

Multiple ST-link Debuggers

Posted on December 23, 2014 at 12:59Hi, I'm debuging a network application running across multiple Nucleo boards with multiple instances of the Keil IDE. Every time a target leaves the debugger the ST-Link connection is lost and reconnection becomes...

occam by Associate II
  • 2655 Views
  • 3 replies
  • 0 kudos

STM32F429 - cannot view external memory in Eclipse memory pane.

Posted on October 24, 2014 at 21:19I have been utilizing Eclipse IDE using GNU tool chain to develop and debug my STM32F429 based project.The target platform has an external SDRAM memory which configured and managed by the MCU's FMC unit. Even thoug...

kurt1 by Associate II
  • 1480 Views
  • 2 replies
  • 0 kudos

stm32 100 I2C peripheral not sending address

Posted on January 07, 2015 at 12:51 I am trying to use the I2C peripheral on the STM32 I am finding that about half the time the address isn't being sent. What happens is that the data line is going low (start condition is set) the clock line go...

SPI clock phase setting

Posted on January 06, 2015 at 09:26I am using STM32L152 part to talk to a digital accelerometer using SPI. The SPI signal timing diagram for the accelerometer is illustrated in the attached figure. Looking at the diagram, it is clear that the spi cl...

bnp979 by Associate III
  • 6620 Views
  • 6 replies
  • 0 kudos

How to declare a big array in external SDRAM?

Posted on January 06, 2015 at 14:03I use STM429 and 128Mb SDRAM and want to decare a big array in keil. How to declare it? How to let keil linker know the array is in external RAM? I defines uint8_t temp[1024*1024], but linker error L6406E: no space...

ray by Associate II
  • 2160 Views
  • 3 replies
  • 0 kudos

Jumpers for STM324x9I-EVAL I/O connectors?

Posted on January 06, 2015 at 15:18These are the 0.05'' (1.27mm) pitch connectors CN6, CN7, CN11 and CN12. The jumpers I normally use on 0.10'' pitch headers are too big to fit. I've done some web searching and not found any jumpers that size. What ...

hbarta2 by Associate III
  • 1379 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.