STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

backup SRAM contents are not retained

Posted on January 09, 2015 at 10:36Hello.I am programming RTC function including time/date and backup SRAM with STM32F407VG.There is a 3.3V battery on the Vbat and a 32.768KHz xtal in my boards.But there are very strange operations in my board.When ...

kbcloud by Associate
  • 999 Views
  • 0 replies
  • 0 kudos

Operation on PC10 causing interference with JTAG comm.?

Posted on January 08, 2015 at 12:38Hello, a while back I encountered a problem where I am unable to JLink-debug my project. Now I have pinpointed the exact line of the problem: GPIO_SetBits   (GPIOC,GPIO_Pin_10); It's a library func. I've checked th...

st-vlink v2 no target connected

Posted on January 07, 2015 at 09:40hi, im trying to connect a STM32F107VCT6 to flash it, but the st-linkv2 doesnt detect it.I have conected pins:4--GROUND6--GROUND7--SWDIO---------------------------PIN 72  MICROCONTROLER8--GROUND9--SECLK------------...

ARM M4 - Timer 2&5 as Encoder Inputs

Posted on January 08, 2015 at 17:14 Hello everyone, Working on a Differentially Steered robot, nothing new (except to me). I found some code on the web that sets up Timer2 in mode3 (Encoder mode) using PA0 & PA1. I have the contents of t...

duane by Associate II
  • 2175 Views
  • 3 replies
  • 0 kudos

STM32F4xx & eMMC

Posted on September 21, 2012 at 21:11Hello all,I have a problem I hope you can help out with. I have grabbed the sample code for writing to an SD card and am modifying it to write to an eMMC chip.In the SD_PowerON() function the original code does a...

dmwarnke by Associate
  • 1587 Views
  • 1 replies
  • 0 kudos

How to change target device in STM32CubeMX

Posted on December 13, 2014 at 00:19How do I change the target device in STM32CubeMX?  Do I need to recreate the entire project and copy over the user sections?  or is there a simple way to do it?Right now, I only want to change from STM32F302R8T6 t...

caleb by Associate III
  • 1898 Views
  • 2 replies
  • 0 kudos

Loosing scope in global variables

Posted on January 08, 2015 at 14:22Hello!I'm using STM32 CubeMX 4.3.1 generating code in Keil. I experienced extrange behavior with Global variables. It seems as if at some point within a function a local variable loses its contents...But debugging ...

edmunoz by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos

STM32 software reset

Posted on January 08, 2015 at 13:46Hello, I want to know what happend when I do a software reset exactlly. I use the function NVIC_SystemReset that set the SYSRESETREQ bit. In the documentation I found:The SYSRESETREQ bit in Cortex™-M4F Application ...

yohann by Associate II
  • 2238 Views
  • 2 replies
  • 0 kudos

Taking microsecond timer without interrupt

Posted on January 08, 2015 at 13:29Hello I'm looking for a solution to get the time between to input signals in microsecond resolution. But I do not want to use an interrupt counting up all microseconds. Is there a convenient solution / method? #...

oli by Associate II
  • 1069 Views
  • 2 replies
  • 0 kudos

[QUESTION] About machine cycle of STM32 and STM8

Posted on January 06, 2015 at 10:30Hello, I want to ask you a question. How many crystal cycles make up a machine cycle are in STM32 and STM8? For example, in 8051, 12 crystal cycles make up 1 machine cycle. Thank you!

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.