STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unstable working of I2S on STM32

Posted on August 08, 2013 at 21:17I faced a critical problem of i2s of STM32.I'm developing a simple system for i2s level meter.MCU - STM32F103RCT6 with external X-tal(12MHz), 72MHz of running clock Inpit Audio - 48KHz, 16bits, stereo i2s digital au...

cubefilm by Associate
  • 2352 Views
  • 4 replies
  • 0 kudos

Vector table relocation

Posted on January 05, 2015 at 17:44I have relocated the Vector Interrupt Table as follows         *((volatile uint32_t *)0xE000ED08) = 0xFFFFFF00 & 0x08004400;                 // jump to bootloader         pVector = GetBootStartEntry();         asm ...

ivesely by Associate II
  • 2849 Views
  • 4 replies
  • 0 kudos

Code generation tool for Std. Peripheral library?

Posted on December 20, 2014 at 16:41Hi everyone,I was wondering if there is a tool like STM32CubeMX to generate initialization code with the standard peripheral library.The Cube is too new and still needs to mature but i do like the STM32CubeMX tool...

STM32L0 GPIOA_MODER A4 default value

Posted on January 06, 2015 at 11:20Hello, the STM32L0 series sets nearly all GPIO to analog mode as default. This does make sense opposed to the ''default to input'' on other family that may result in high current draw with floating inputs. Only Por...

SPI input value being interpreted incorrectly

Posted on January 04, 2015 at 04:11My project involves using a STM32L152 part as a SPI master that receives data from a slave (digital accelerometer). When I look at the SPI signals through a scope, I notice that the incoming SPI data is being inter...

bnp979 by Associate III
  • 4811 Views
  • 5 replies
  • 0 kudos

STM32F4 Discovery and gnu

Posted on January 05, 2015 at 14:21I have a new STM32f4 Discovery board and would like to be able to build, burn, debug programs in Ubuntu linux version 14.04. I basically followed these directions: http://www.wolinlabs.com/blog/linux.stm32.discover...

bobslf by Associate
  • 1388 Views
  • 1 replies
  • 0 kudos

configure LSE for RTC on a STM32F4DISCOVERY board.

Posted on January 01, 2015 at 09:39Hello, hapy 2015 to all. I try to use an external LSE for RTC a STM32F4DISCOVERY . I follow indication of clive1 on this post: https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder...

stm32f4 by Associate II
  • 2502 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.