cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L-Discovery communicate in I2C with M24LR64

Posted on April 24, 2012 at 09:13

Hello everybody,

I have some troubel to communicate with m24LR64. I use a STM32L- Discovery.

I try to see something in the oscilloscope but nothing, could you help me to see what is wrong in my code:

#define I2C2_SLAVE_ADDRESS7     0xA0   // EEPROM I2C Address

#define ClockSpeed              200000 // 200 KHz

#include ''mainsee.h''

void I2Cmain(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

I2C_InitTypeDef  I2C_InitStructure;

       

  /* I2C1 and I2C2 Periph clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);

  /* GPIOB Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

 

  /* Configure I2C2 pins: SCL and SDA ----------------------------------------*/

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_10 | GPIO_Pin_11;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_OD;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_10, GPIO_AF_I2C2);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_11, GPIO_AF_I2C2);

  //I2C_DeInit(I2C2);    

           

  /* I2C2 configuration ------------------------------------------------------*/

  I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

  I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

  I2C_InitStructure.I2C_OwnAddress1 = I2C2_SLAVE_ADDRESS7;

  I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

  I2C_InitStructure.I2C_ClockSpeed = ClockSpeed;

  I2C_Init(I2C2, &I2C_InitStructure);

  /* Enable I2C2 -------------------------------------------------------------*/

  I2C_Cmd(I2C2, ENABLE);

  /* Send I2C1 START condition */

  I2C_GenerateSTART(I2C2, ENABLE);

  /* Test on I2C1 EV5 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT));

   /* Send EEPROM slave Address for write */

  //I2C_Send7bitAddress(I2C2, I2C2_SLAVE_ADDRESS7, I2C_Direction_Transmitter);  }

  /* Test on I2C1 EV6 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

 while(1){

  /* Send I2C1 EEPROM internal address */

  I2C_SendData(I2C2, 0x00);   }

  /* Test on I2C1 EV8 and clear it */

  while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 EEPROM data */

  I2C_SendData(I2C2, 0x05);

  /* Test on I2C1 EV8 and clear it */

  while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 STOP Condition */

  I2C_GenerateSTOP(I2C2, ENABLE);

  while(1); // Do not exit

}

Thank you very much in advance to help me.

P.S: Sorry for the english, i'm French.

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on April 24, 2012 at 13:39

Start by moving I2C_Cmd(I2C2, ENABLE); before the I2C_Init()

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on April 24, 2012 at 14:26

No change unfortunately, I've read some post to configure the I2C and i've make like in this post, but nothing in oscilloscope. Pull-up resistori is needed? even with, no change.

It's curious because one month ago i manged to have SCL and SDA for different value of data, but now tha i have m24Lr, it doesn't work. plug or not this the same.

alok472
Associate II
Posted on April 24, 2012 at 15:24

Yes, Pull-up are needed on I2C bus.

Did you try to run the standard peripheral example on I2C ?

Eventually you may have to uncomment the code for sending the I2C Address

Posted on April 24, 2012 at 15:43

I've tried with resistor but one month ago when it works i don't have pull up resistor.

i have find in library code for i2C with the M24LR64, but it use some function that it don't implement with the library stm32l152_eval_i2c_ee.c, i had come difficulties to add it, but even with the result are the same.

sEE_Init();

  sEE_WriteBuffer(Tx1_Buffer, sEE_WRITE_ADDRESS1, BUFFER_SIZE1); /* première écriture */

  sEE_WaitEepromStandbyState();     /* Wait for EEPROM standby state */

  NumDataRead = BUFFER_SIZE1; /* Set the Number of data to be read */                                                                             

  sEE_ReadBuffer(Rx1_Buffer, sEE_READ_ADDRESS1, (uint16_t *)(&NumDataRead)); /* Read from I2C EEPROM from sEE_READ_ADDRESS1 */

  LCD_GLASS_DisplayString(''T1 ONGOING'');

  while (NumDataRead > 0)

  {}        

  TransferStatus1 = Buffercmp(Tx1_Buffer, Rx1_Buffer, BUFFER_SIZE1); /* Check if the data written to the memory is read correctly */

  /* TransferStatus1 = PASSED, if the transmitted and received data to/from the EEPROM are the same */

  /* TransferStatus1 = FAILED, if the transmitted and received data to/from the EEPROM are different */

  if (TransferStatus1 == PASSED)

  {

    LCD_GLASS_DisplayString(''T1 PASS'');

  }

  else

  {

    LCD_GLASS_DisplayString(''T1 FAIL'');

  }

 

  sEE_WriteBuffer(Tx2_Buffer, sEE_WRITE_ADDRESS2, BUFFER_SIZE2);        /* Second write in the memory followed by a read of the written data -------*/

  sEE_WaitEepromStandbyState();  /* Wait for EEPROM standby state */  

  NumDataRead = BUFFER_SIZE2;/* Set the Number of data to be read */   

  sEE_ReadBuffer(Rx2_Buffer, sEE_READ_ADDRESS2, (uint16_t *)(&NumDataRead)); /* Read from I2C EEPROM from sEE_READ_ADDRESS2 */

  LCD_GLASS_DisplayString(''T2 ONGOING'');

  /* Wait till DMA transfer is compelete (Tranfer complete interrupt handler resets the variable holding the number of data to be read) */

 while (NumDataRead > 0)

 {}      

  TransferStatus2 = Buffercmp(Tx2_Buffer, Rx2_Buffer, BUFFER_SIZE2);/* Check if the data written to the memory is read correctly */

  /* TransferStatus2 = PASSED, if the transmitted and received data to/from the EEPROM are the same */

  /* TransferStatus2 = FAILED, if the transmitted and received data to/from the EEPROM are different */

  if (TransferStatus2 == PASSED)

  {

    LCD_GLASS_DisplayString(''T2 PASS'');

  }

  else

  {

    LCD_GLASS_DisplayString(''T2 FAIL'');

  }

  sEE_DeInit();

        

   while(1)

   { }

}

TestStatus Buffercmp(uint8_t* pBuffer1, uint8_t* pBuffer2, uint16_t BufferLength)

{

  while(BufferLength--)

  {

    if(*pBuffer1 != *pBuffer2)

    {

      return FAILED;

    }

    

    pBuffer1++;

    pBuffer2++;

  }

  return PASSED;  

}

simonlee0311
Associate II
Posted on April 24, 2012 at 15:48

Hi!!

Yes. You need to add the Pull-high resistor on SDA and SCL pin.

You can try official sample code to try it.

I also try it before, and it will more quickly to know the setting of I2C function on STM32.

Posted on April 24, 2012 at 15:56

and what value of the resistor i have to make?

i keep this?

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

alok472
Associate II
Posted on April 24, 2012 at 19:23

Yes, the settings are fine.

I normally use 4.7K. I will suggest a value between 2.2K to 10K.

Posted on April 25, 2012 at 09:12

Good morning everybody!

No change this morning even with the resistor. Before the programme are running the two signal are at 3.3V, and at the moment of i push for run the two signals begin to 0V.

I

gives

the code

in case

an error

that would

drag

.

void I2Cmain(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

I2C_InitTypeDef  I2C_InitStructure;

           

  /* I2C1 and I2C2 Periph clock enable */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C2, ENABLE);

  /* GPIOB Periph clock enable */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);  

 

  /* Configure I2C2 pins: SCL and SDA ----------------------------------------*/

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_10 | GPIO_Pin_11;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOB, &GPIO_InitStructure);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_10, GPIO_AF_I2C2);

  GPIO_PinAFConfig(GPIOB, GPIO_Pin_11, GPIO_AF_I2C2);

  /* Enable I2C2 -------------------------------------------------------------*/

  //I2C_DeInit(I2C2);    

  I2C_Cmd(I2C2, ENABLE);  

           

  /* I2C2 configuration ------------------------------------------------------*/

  I2C_InitStructure.I2C_Mode = I2C_Mode_I2C;

  I2C_InitStructure.I2C_DutyCycle = I2C_DutyCycle_2;

  I2C_InitStructure.I2C_OwnAddress1 = 0xA0;

  I2C_InitStructure.I2C_Ack = I2C_Ack_Enable;

  I2C_InitStructure.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit;

  I2C_InitStructure.I2C_ClockSpeed = ClockSpeed;

  I2C_Init(I2C2, &I2C_InitStructure);

  //I2C_StretchClockCmd(I2C2,ENABLE);

 while(1){

  /* Send I2C1 START condition */

  I2C_GenerateSTART(I2C2, ENABLE);

  /* Test on I2C1 EV5 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT));

   /* Send EEPROM slave Address for write */

  I2C_Send7bitAddress(I2C2, I2C2_SLAVE_ADDRESS7, I2C_Direction_Transmitter);  

  /* Test on I2C1 EV6 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));

  /* Send I2C1 EEPROM internal address */

  I2C_SendData(I2C2, 0x00);   

  /* Test on I2C1 EV8 and clear it */

 // while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 EEPROM data */

  I2C_SendData(I2C2, 0x05);

  /* Test on I2C1 EV8 and clear it */

  //while(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED));

  /* Send I2C1 STOP Condition */

  I2C_GenerateSTOP(I2C2, ENABLE);

  }

 

}

Posted on April 26, 2012 at 08:16

hi,

No error in my code? I've pull up resistor of 4k7.

I really don't know why it doesn't wor, i need your help.

thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.