STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX 4.15.0 Bug Report

Posted on May 29, 2016 at 20:02When some output configured as an alternative function, the only option available is ''Alternative Function Push Pull'' but according to Ref manual (e.g. for stm32f405) the Open Drain for alternative function is also p...

megaboy2k by Associate II
  • 4430 Views
  • 11 replies
  • 0 kudos

What memories does video playback in F746 Discovery use?

Posted on June 02, 2016 at 19:19I thought I would clone part of the STM32F746 Discovery board to show a simple video (and other things). I also noticed that the board has external SDram and flashrom. To be absolutely sure and before I start, I want ...

LMI2 by Lead
  • 677 Views
  • 0 replies
  • 0 kudos

STM32F302 Clock Configuration

Posted on May 21, 2016 at 03:37I am trying to get the Clock Configuration of an STM32F302CB to work. We are using 16 MHz Oscillators. With the STM32F4 I used the clock configuration tool to generate the system_stm32xxx.c file. Unfortunately, I did n...

DMA Memory To UART5

Posted on June 25, 2012 at 15:38 Hi, I'm having an issue setting up a DMA to transfer data from a 2 element uint8_t array to UART5. The code works, but the UART only sends out the first byte and having tried lots of different thing...

dclark9 by Associate II
  • 10488 Views
  • 29 replies
  • 0 kudos

Don't working USART in STM32F051K8U6

Posted on May 30, 2016 at 21:58Hello. I'm use MCU STM32F051K8U6 for simple devices.I'm had a problem when using the UART.If i'm initialize USART thus (with SPL):It freezes the microcontroller, and the program is not executed.void GPIO_Initialization...

s9 by Associate II
  • 2493 Views
  • 5 replies
  • 0 kudos

Keil uvision debug script

Posted on May 12, 2014 at 14:19Hello,is there a possibility to make debuging scripts for STM32 processors in Keil uvision MDK? 

hospodar by Associate III
  • 1484 Views
  • 2 replies
  • 0 kudos

STM32L1 internal EEprom (user data in NVM)

Posted on May 29, 2016 at 23:18In STM32L1 how works the internal small EEPROM? (The Data EEPROM memory block. It contains user data)For example the Page 0 0x0800 0000 - 0x0800 00FF = 256 bytes, to use it must be first erased?For write is DATA_EEPROM...

Questions on what's happning before main() is called

Posted on June 01, 2016 at 16:19 I am working with the STM32F405/STM32F407 microcontrollers.I am trying to understand what's happening inside the microcontroller before main() is called and I would like to get rid of as much as possible to minim...

arnold_w by Senior II
  • 1849 Views
  • 4 replies
  • 0 kudos

Step+Dir Interface to STM32F4

Posted on May 30, 2016 at 05:42Hello, i am in the path of developing brush-less DC servo system for CNC mill, Because i will use motor encoder, as well as position quadrature encoder, i need ability of hardware tracking step and dir impulses. It wo...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.