2016-06-02 2:13 AM
Hello Everyone,
I have implemented a ADC conversion of 6 Analog Voltages, 2 on each ADC1,2,3. They are running in Triple Mode and The DMA2 is writing them to a buffer. With the DMA Complete Interrupt i copy the Buffer to wherever i want him. The Problem I have is that the order i expect the results to be in the buffer is different. According to the manual they are supposed to be in the order: ADC1.1 ADC 2.1 ADC3.1 ADC 1.2 ADC 2.2 ADC 3.2. I write them to a 6 element uint16 buffer while the DMA is ordered to transfer 3 uint32 bit values to a 3 element 32 bit buffer. I think that should not be a problem. My results though show, that the first two values to be converted somehow show up in the 2nd ord 3rd word, meaning at position 3,4 or 5,6 in my buffer. If I have 56cycles adc conversion its 3,4 If I have 84cycles adc conversion its 5,6 Can someone tell my how I can fix this, or if this will be at least fix so i can just implement another order of reading them and be done with it. thanks.int main(void)
{
/*------------------------------------------------------------------------*
*--- Systemclock = 168MHz -----------------------------------------------*
*--- Systemclock / 80kHz == Number of steps for up and down counting ----*
*--- Timer1_Steps = Systemclock / (2*80kHz) - 1 Maximum Counter value ---*
*----Timer1_Steps = 1049 ------------------------------------------------*
*------------------------------------------------------------------------*/
/*--- Initializing Pins --------------------*/
init_pins();
init_pwm_pins();
init_adc_pins();
/*--- Initializing ADCs --------------------*/
init_dma2_C0();
init_ADC123();
/*--- Initializing Timers ------------------*/
StartTimer1(Timer1_Steps, 0);
Init_TIM1PWM(50); // 50 == 300ns deadtime
//set_CCR(1000, 50, 500);
StartTimer3(20000,4667,5000,10000,15000,0);
StartTimer4(359,Timer4_Prescaler);
//CCR1 = 1000;
//CCR2 = 50;
//CCR3 = 500;
while (1)
{
}//while(1)
}//main
/*--- ADC Pin Init --------------------------------*/
void init_adc_pins(){
/*u3 -> PC0 ADC123_IN10
u2 -> PB1 ADC12_IN9
u1 -> PB0 ADC12_IN8
i3 -> PA3 ADC123_IN3
i2 -> PA2 ADC123_IN2
i1 -> PA1 ADC123_IN1*/
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
/*--- Configure PB -------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/*--- Configure PA -------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/*--- Configure PC -------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_Init(GPIOC, &GPIO_InitStructure);
}
void init_dma2_C0(){
extern uint16_t ADC_BUFF[bufferlength];
DMA_InitTypeDef DMA_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
/*--- Enable the DMA2 gloabal Interrupt -----------*/
NVIC_InitStructure.NVIC_IRQChannel = DMA2_Stream0_IRQn ;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 2;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
DMA_DeInit(DMA2_Stream0);
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&(ADC->CDR);
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t) &ADC_BUFF;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = bufferlength/2;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Word;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Word; //Half-Word
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;//Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_3QuartersFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
DMA_ITConfig(DMA2_Stream0, DMA_IT_TC, ENABLE);
DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_TCIF0);
DMA_Cmd(DMA2_Stream0, ENABLE);
}
void init_ADC123(){
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
/*u3 -> PC0 ADC123_IN10
u2 -> PB1 ADC12_IN9
u1 -> PB0 ADC12_IN8
i3 -> PA3 ADC123_IN3
i2 -> PA2 ADC123_IN2
i1 -> PA1 ADC123_IN1*/
/*--- Periperal clock enable ---------------*/
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE);
/*--- struct to default settings -----------*/
ADC_StructInit(&ADC_InitStructure);
ADC_DeInit();
/*--- ADC1 Configuration -------------------*/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 2;//adc_samples;
ADC_Init(ADC1, &ADC_InitStructure);
/*--- ADC2 Configuration -------------------*/
ADC_Init(ADC2, &ADC_InitStructure);
/*--- ADC3 Configuration -------------------*/
ADC_Init(ADC3, &ADC_InitStructure);
/*--- ADC Common configuration -------------*/
ADC_CommonInitStructure.ADC_Mode = ADC_TripleMode_Interl;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_20Cycles;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_2;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInit(&ADC_CommonInitStructure);
/*--- configuration of ADC1 channel ranks --*/
/*--- u1 / u2 ---*/
ADC_RegularChannelConfig(ADC1,ADC_Channel_8,1,ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC1,ADC_Channel_9,2,ADC_SampleTime_56Cycles);
/*--- configuration of ADC2 channel ranks --*/
/*--- i1 / i2 ---*/
ADC_RegularChannelConfig(ADC2,ADC_Channel_1,1,ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC2,ADC_Channel_2,2,ADC_SampleTime_56Cycles);
/*--- configuration of ADC3 channel ranks --*/
/*--- u3 / i3 ---*/
ADC_RegularChannelConfig(ADC3,ADC_Channel_10,1,ADC_SampleTime_56Cycles);
ADC_RegularChannelConfig(ADC3,ADC_Channel_3,2,ADC_SampleTime_56Cycles);
/*--- Enable ADC1 - ADC 3 ------------------*/
ADC_Cmd(ADC1, ENABLE);
ADC_Cmd(ADC2, ENABLE);
ADC_Cmd(ADC3, ENABLE);
/*--- Enable multi ADC DMA requests --------*/
ADC_MultiModeDMARequestAfterLastTransferCmd(ENABLE);
ADC_DMACmd(ADC1, ENABLE);
/*--- Starting of ADC conversion -----------*/
ADC_SoftwareStartConv(ADC1);
ADC_SoftwareStartConv(ADC2);
ADC_SoftwareStartConv(ADC3);
}
void DMA2_Stream0_IRQHandler(void){
//volatile uint16_t test=1367;
//DMA_Cmd(DMA2_Stream0, DISABLE);
if(DMA_GetITStatus(DMA2_Stream0,DMA_IT_TCIF0))
{
DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_TCIF0);
if(ADC_wp == ADC_meanlength) ADC_wp=0;
ADC_result[0][ADC_wp]=ADC_BUFF[2];//B0 //u1 1349 1345
ADC_result[1][ADC_wp]=ADC_BUFF[5];//B1 //u2 958 954
ADC_result[2][ADC_wp]=ADC_BUFF[4];//C0 //u3 4095 4095
ADC_result[3][ADC_wp]=ADC_BUFF[3];//A1 //i1 286 278
ADC_result[4][ADC_wp]=ADC_BUFF[0];//A2 //i2 3576 3552
ADC_result[5][ADC_wp]=ADC_BUFF[1];//A3 //i3 1 0
GPIO_ToggleBits(GPIOD,GPIO_Pin_13);
if(testflag == 0){
test[0][testflag1] = ADC_result[4][ADC_wp];//ADC_values[0];
test[1][testflag1] = ADC_result[5][ADC_wp];//ADC_values[1];
test[2][testflag1] = ADC_result[0][ADC_wp];//ADC_values[2];
test[3][testflag1] = ADC_result[3][ADC_wp];//ADC_values[3];
test[4][testflag1] = ADC_result[2][ADC_wp];//ADC_values[4];
test[5][testflag1] = ADC_result[1][ADC_wp];//ADC_values[5];
testflag=0;
testflag1++;
if(testflag1 == 100)testflag1 = 0;
}
else testflag++;
/*
*/
ADC_wp++;
}
}
2016-06-02 9:05 AM
Pretty sure I've posted working examples.Observe how I post complete code for my examples, I'm not looking to fix everyone else's broken code.For short buffers I'd be wary of the FIFO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.