STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DS1307 RTC + STM32F4 + HAL LIB

Posted on May 28, 2016 at 01:53Hi,I am working on STM32F4 Discovery. I need help in interfacing DS1307 RTC with Controller using HAL Library. Please if anyone can help!ThanksAnuj #!stm32f4 #!stm32-!cubemx-!rtc

anuj by Associate II
  • 3382 Views
  • 2 replies
  • 0 kudos

working with stm32f3 development board and st7565R

Posted on June 04, 2016 at 16:10 Hi, I'm trying to initialize the the graphic LCD ST7565R in spi mode the connections are as per the datasheet. Used the 1uf capacitors bw cap2n-cap2p,cap1n-cap1p,cap1n-cap3p,vout-vss,v0-vss,v1-vss,v2-vss,v3-vs...

STM32F0 ms5611 I2C HAL problem

Posted on June 04, 2016 at 12:40 Hi i have problem with communication with ms5611 pressure sensor by I2C HAL library. Algorithms used to read registers look like in documentation: http://www.meas-spec.com/downloads/MS5611-01BApdf I done s...

starcu93 by Associate
  • 1341 Views
  • 0 replies
  • 0 kudos

Keil C Lost Libraries Just Added

Posted on June 03, 2016 at 11:59At the first i created a new project by STM cube. And using in Keil C, i added another library into my KIEL C. when i re-build again my STM cube all my libraries is gone. How can i solve it.

Cube USART DMA Tranfer works only once.

Posted on June 03, 2016 at 22:35Hi everybody, I have some issue with using the DMA Transfer method on a Discovery F3 (F303) board. Don't know if it's a bug, or if I missed something... The HAL is generated with Cube (under Eclipse, Cube-Version is S...

STM32F407VE and CAN2 is impossible to initialize

Posted on June 02, 2016 at 14:52Hello. I have initialized CAN1 and it works properly. I need initialize after a while CAN2 and it is finishing on timeout because INAK is stil TRUE. Where can be problem? Thanks, Jiri #can2-stm32f407-inak

Unable to download any CubeMX package!!

Posted on June 03, 2016 at 11:22Tried to download CubeMX 4.15 but couldn't find it. Neither is it possible to download the CubeMxF1 package or the CubeMxF2 package!! It seems that all the download links are dead!!

Check CAN on single nucleo F103

Posted on June 02, 2016 at 08:24Hi everyone.I see CAN TX interrups.I can't catch interrupt related to CAN RX just by putting jumper between PB8 and PB9 (GPIOs are remapped - double checked).Is it possible ? #bxcan #nucleo103rb #stm32 #can

Interfacing external SRAM STM32F205ZCT6

Posted on June 01, 2016 at 06:41In one of application I need to hold large amount of data in SRAM around 20MB.Which external SRAM should be used & any example code for interfacing it with STM32F205ZCT6. External SRAM required only for data holding f...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.