2014-05-12 5:19 AM
Hello,
is there a possibility to make debuging scripts for STM32 processors in Keil uvision MDK?2014-05-21 9:01 AM
Hi hospodar.ivan,
This is possible! You can find helpful documentation on ARM web site for :Scripting langage:
http://www.keil.com/support/man/docs/uv4/uv4_debug_functions.htm
Debug from command line
:
http://www.keil.com/support/man/docs/uv4/uv4_commandline.htm
Best Regards, Nouha2016-06-02 7:29 AM
Hi,
I would like to write debug/signal functions for my STM32F429I discovery board. Unfortunately the Debugger complains with ''undefined identifier'' for any input or output register, e.g. S0IN or AIN0.When I execute ''DIR VTREG'', the debugger outputs the following result.
TRAPS: ulong, value = 0x00000000
TRIGFLT: ulong, value = 0x00000000STCLK: ulong, value = 0x00000000XTAL: ulong, value = 0x007A1200CLOCK: ulong, value = 0x007A1200Does this mean, the registers for ADC, Serial Port or the GPIO's are not supported? The project was generated using STM32CubeMX.
Thanks in advance for any support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.