STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to utilize 4.2MB RAM in STM32N6

Hi,I am using STM32N6570-DK kit. In my application I need ~3.5MB of RAM but if I allocate more than 256KB of RAM I get the error "region `RAM' overflowed by xxxx bytes".  I got the same results as well when I imported "UART_HyperTerminal_IT" example ...

Jayesh2 by Associate II
  • 5169 Views
  • 6 replies
  • 2 kudos

STM32H747 - DSI overflow error, no video output

Greetings!I have a board with STM32H747XI and SN65DSI84-Q1 as a converter from DSI to LVDS.The issue is that I can not get video output from MCU to 2ch LVDS panel 1920x720 with any configuration I'm trying. The main issue is that I'm getting HAL_DSI_...

VHEMaster by Associate III
  • 5581 Views
  • 10 replies
  • 0 kudos

Resolved! STM32h7 SPI DMA communication issues + FIFO Error (FEIF)

When using DMA to do a SPI transmit, I found a strange behavior. The problem is, that the communication to the DAC works for a few seconds, depending on the used frequency. After the few seconds only 1 byte instead of 3 bytes are sent and the NSS Pin...

Heiko_SM by Associate II
  • 7280 Views
  • 7 replies
  • 0 kudos

STM32F4 & STM32F7 USB Host Core (Interrupt flood)

Posted on May 19, 2017 at 01:02Issue:USB Core issing interrupt at a rate of 8.65us causing high CPU loading.Software/Chip:Using USB Host/CDC from STM32Cube V1.15 on a STM32F429 board.   USB interrupt sources:- SOF Interrupts (It is not needed for CD...

Resolved! Processor pin assignments

Given an MCU (say an STM32H755ZIT) and a function (say SPI2_MOSI), how can you find which pins may be configured as SPI2_MOSI, short of clicking on every pin in the Pinout View of the MX Device Configuration Tools?

SoCalJim by Associate III
  • 2096 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.