STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC DMA TIM - U5XX Family

Good afternoon,  I have a question regarding the best strategy to follow on how to measure multiple channels with the ADC (triggered with timer) and map them to the DMA. I have followed the project called ADC_DMA_Transfer that can be found in the Pro...

Marc3 by Associate III
  • 1220 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H733 data cache initialization issue

Hello,I am using a STM32H733VGT on a custom design board. On a fresh project in CubeMX, I tried to activate data cache but the autogenerated code crashes at  SCB_EnableDCache(); . (nothing has been activated on the CubeMX, just the external crystal a...

amirshn by Associate III
  • 5077 Views
  • 9 replies
  • 1 kudos

Resolved! TIMER - Overflow event - Must reset CNT?

Hi There,I have setup TIMER4 on STM32G484 device for overflow event and enabled interrupt for events. Everything works fine and as expected with correct fire time if I RESET the CNT register in the ISR. However, if I do not, it seems to do some level...

Skeeb by Associate II
  • 2349 Views
  • 5 replies
  • 0 kudos

STM32f407 boot mode

Hi I am using STM32F407 DISCOVERY BOARD and I am able to make the board change to boot mode using a another controller.After boot mode change over I need to program the memory of STM32F407 DISCOVERY BOARD by UART communication.Here I am unable to get...

AKHIL6 by Associate II
  • 1357 Views
  • 2 replies
  • 0 kudos

Resolved! How to debug a hard fault exception for STM32?

I am currently using stm32f407 with FreeRTOS as operating system in MDK IDE. Recently, When I added a new function ( The new function is ospf routing algorithm, and it is very complex and involves many files ) to my project, I began to encounter hard...

yanhc by Associate III
  • 14076 Views
  • 13 replies
  • 0 kudos

Resolved! Bootloader startup time on STM32L4R

This is mostly a post to help people who try to google this later since I couldn't find anything. If you look at AN2606 table 197, it lists the minimum startup time for the bootloader on a bunch of different STM32 microcontrollers. For some reason, j...

Resolved! STM32L47 Bootloader v9.x SPI bug

Recently, I have been working on a project that intends to utilize the v9.x bootloader on an STM32L471VGT6 through the SPI 2 port. When utilizing the write memory command, I would find that the STM32L4 would occasionally have 0xFFFFFFFFFFFFFFFF writt...

chaup by Associate II
  • 2127 Views
  • 2 replies
  • 1 kudos

Resolved! Using SPI on STM32H7 in mixed mode, normal and DMA.

I am working on a STM32H723 microcontroller and I am trying to use and SPI communication in mixed mode, i.e. normal and DMA.The reason I need this is because I have a third party software stack for a device that is set up in a certain way, and it cyc...

ioncasu by Associate II
  • 3495 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.