STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Stuck in boot mode

I'm using the STM32H753ZIT6 NUCLEO Board. For some reason the User LED's are on by default even without any code on it. I tried to press the reset button but it would just blink the led's. I read on another forum to short the BOOT0 and Vdd pins but w...

LopsidedCoder_0-1739809281448.jpeg

STM32G0B0RET6 failure rate

We are on the second generation of prototype here. On the first generation I had an MCU fail for reasons I couldn't trace.  This was from a set of six. I have now powered seven of the second generation two have had MCU failures.  The second failure w...

Zdiode by Associate II
  • 5105 Views
  • 10 replies
  • 5 kudos

Resolved! How to disable XSPI SCK Clock preamble?

Good day Folks,I am hoping you are able to shed some light on this odd XSPI clock behaviour.  I have connected XSPI2 to a W25Q64 Flash in QSPI mode.There are 'preamble' clocks present prior to the NCS being asserted. I've noticed that the number of p...

exarian_0-1739629846858.png exarian_1-1739630051967.png exarian_2-1739630122997.png exarian_3-1739630235507.png
exarian by Associate III
  • 1451 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H745 Bootloader and RAM on STM32H745XI-DISCO

I want to create and application on a STM32H745XI-DISCO. I am not using M7 core only M4.Reference manual says that upto 864kB of SRAM  and 2MB of flash are available.I will receive the application sw via Can. My bootloader will save it RAM and after ...

ADC Multichannel - DMA on STM32U545

Good afternoon,  I have some questions for reading multiple channels of the ADC in continuous mode and map the results in the DMA. I have been able to monitor the voltage coming from a potentiometer and map it into the DMA and i can see the values in...

Marc3 by Associate III
  • 2051 Views
  • 4 replies
  • 0 kudos

Resolved! ADC - DMA - TIM

Hello everyone  New STM32 user here, more specifically STM32 U545 RE-Q. I am kind of new and i would like to start acquiring some data with the STM32 ADC, triggered by a timer, and send the data to the DMA so that i can use the CPU for other stuff. D...

Marc3 by Associate III
  • 1371 Views
  • 1 replies
  • 1 kudos

Resolved! I2C Slave device implementation ACK/NACK problem

As mentioned in the topic subject, I would like to implement I2C Slave device which will simulate the BQ769x2 device. For development I'm using STM32F4 Discovery board, but the final product will be deployed on STM32L0.Master device is first trying t...

mr4k_0-1739542590631.png Write_3E_0100_NACK1.png Write_3E_0100_ACK.png
mr4k by Associate II
  • 2415 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.